Grettings We have in the field a PF755 drive connected to an 32 poles permanet magnet motor using the PCP oil well application. The motor runs unstable as if it has a fisical impediment in the bearing. The torque shown in the parameter 1166 vary from 0 to 300 to 0 again in a matter of seconds. Originally ...
|