List of Contributions

BWilken

Contact Details

BWilken


My Content

1 to 13 of 13 total
Posted By BWilken Dec 04, 2025 10:07:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you GLaDOS, I had reviewed that manual and did not see anything that seemed to concern me. However, I spoke with the product specialist with our Vendor and they are who led me to believe it could be a potential issue worth researching, I just can't seem to find any more information one way or the ...
Posted By BWilken Dec 04, 2025 08:26:00 AM
Found In Egroup: Automation Control
\ view thread
I have a system with an L55 controller that is currently SIL2, I need to upgrade this controller due to obsolescence. The most practical option right now is to upgrade to an L71. I am looking for documentation that would assist me in confirming if there are any specific configuration changes I will need ...
Posted By BWilken May 02, 2025 11:54:00 AM
Found In Egroup: Automation Control
\ view thread
lost an old PanielView 900 on a SLC, as a short term resolution trying to set up a pv + 1250 to use in its place. Original Connection is RS 232 and only option available for time being. I had to convert an old .pva file so I could use FTV Studio and it lost the Comms settings in the covnersion so I believe ...
Posted By BWilken May 01, 2025 12:37:00 PM
Found In Egroup: Automation Control
\ view thread
Have a SLC processor attempting to replace an antiquated HMI with a PanelView Plus 7 via the existing DF1 (RS 232) connection, is this possible? Alternatively we have a PanelView plus 1250 with a logic module that has the RS 232 connection but we cannot seem to get the FactoryTalk Links Configurations ...
Posted By BWilken Apr 14, 2025 10:38:00 AM
Found In Egroup: Installation & Activation
\ view thread
Hello, I am attempting to activate a license on an offline PC and using an online PC. I have followed the steps described in the procedure. At this point it is displaying that I should be able to change binding location to, howver this is gray and does not give me the option to do so, anyone ran into ...
Posted By BWilken Feb 24, 2023 07:07:00 AM
Found In Egroup: Legacy
\ view thread
I'm not sure I can give a solid explanation but via the io config tab there is an option to see the "estimated" current load which I assume is calculated based on the specific load of each current added to the IO rack in the program. In our case the max was 2amp and we that was calculated to exceed by ...
Posted By BWilken Feb 23, 2023 05:52:00 AM
Found In Egroup: Legacy
\ view thread
Follow up on this issue, turned out to be power supply was bad. Long story short but PLC has been in service for nearly 20 years, looking at power supply loading via IO config the calculated load exceeded the recommended load by about 350mA. I suppose after 20 years this may have finally caught up and, ...
Posted By BWilken Feb 14, 2023 07:25:00 AM
Found In Egroup: Legacy
\ view thread
Thanks for the feedback, going to swap the backplane today to rule it out. This particular rack has been running for over 20 years on the same program, and these issues just began 3 days ago, hopefully this will resolve. Going to set some traps with time stamps on these outputs and the logic that triggers, ...
Posted By BWilken Feb 13, 2023 10:07:00 AM
Found In Egroup: Legacy
\ view thread
Good Day, I have an SLC 500, well several actually, but still more familiar with the modern stuff. Wandering if there are any tools I may be not aware of to help troubleshoot some mysteries. Potentially an issue with back plane, have 2 separate isolated relay outputs cards with separate power supplies, ...
Posted By BWilken Apr 21, 2022 12:44:00 PM
Found In Egroup: Installation & Activation
\ view thread
Thanks for your response Filip. Would you mind a brief explanation for your recommendation against using a VM to host? Unfortunately I am not sure this is an option in our case...so just curious as to what conflicts it would cause
Posted By BWilken Apr 21, 2022 10:12:00 AM
Found In Egroup: Installation & Activation
\ view thread
I am tying to find some guidance to create a network license server that can host multiples of the same licenses for use while on network or to check out. I have used this before however I not from the administrator side. I currently have an exclusive VM which will host the Factory Talk Activation Manager, ...
Posted By BWilken Mar 31, 2022 05:38:00 AM
Found In Egroup: Automation Control
\ view thread
Thanks for feedback, I did end up just replacing the HMI with a new one, however I was just hoping maybe in my downtime I could get the old one up to date and put it on the spare rack being that it is still in great condition. Might just replace logic module as you suggested. Thanks!
Posted By BWilken Mar 30, 2022 12:42:00 PM
Found In Egroup: Automation Control
\ view thread
Hello, I have an old panelvew plus 1250 with v 3.2 firmware. In order to used an edited FTV program from latest FTV software I must have a version no later than 6.2. I have looked on Rockwell download center and (panelview plus 600-1500) firmware is all discontinued, and only up to 5.1 anyway. Can I ...