Posted By
Rao
Oct 02, 2025 04:19:00 AM
Found In
Egroup:
Automation Control
\
view thread
Dear Experts, One of the Customer at site has Ungrounded Neutral UPS system. Voltage measured are : L&N=110VAC, N&G=55VAC, L&G=55VAC. I am not clear if 1756-PA75 supports Ungrounded Neutral at the Input side without any need for external Isolation Transformer at the Upstream of of 1756-PA75? The ...
|