List of Contributions

Haglund

Contact Details

Haglund


My Content

1 to 10 of 10 total
Posted By Haglund Oct 31, 2025 08:23:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
@asemlucben But it will be resolved before 1.7 release? -------------------------------------------
Posted By Haglund Oct 31, 2025 08:18:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
@asemlucben but according to the code it should be at the right, or am I missing something? yAxis.Position = HorizontalPosition.Right;-------------------------------------------
Posted By Haglund Oct 31, 2025 05:46:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I just got a beta of 1.7 (FTOptixStudioSetup_Win32_1.7.0.480.Beta) and tested this. I tested the small application I added in the thread + trend_pens_runtime and none of them works with this beta either. So from my understanding the bug is still there. Has anyone at ASEM looked more into ...
Posted By Haglund Oct 09, 2025 01:30:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Do you have any more information about this anomaly or a pre version of 1.7 so I could verify that it resolves my issue when released? -------------------------------------------
Posted By Haglund Oct 09, 2025 01:03:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, Strange, so you get an Y-Axis to the right in the trend, not the left(default) as it will be when it doesn't use the attached Y-Axis? When I try it I do only get the Y-Axis to the left, not to the right as it should be if it was from the code. -------------------------------------------
Posted By Haglund Oct 08, 2025 09:40:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, I did some tests with your project and the Y-Axis is not added from the code. Even if I comment away the Y-Axis part in code it gets a separate axis in the trend (a part from that the trend does not change position of the axis when changed it in the code either). When I opened the project ...
Posted By Haglund Oct 08, 2025 01:24:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thank you, I created a minimal project with the separate y axis for the pens like I try to do. Might help if I have missed something, from my understanding this should make separate Y axis for all pens to the right. -------------------------------------------
Posted By Haglund Oct 07, 2025 10:03:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, NameSpaceIndex for the object type is 8 as in your picture. the one on the right is the one not working (and does not go to attached status). I use the Owner.Get to find all objects needed in this case as well. -------------------------------------------
Posted By Haglund Oct 07, 2025 08:55:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, I am using FT Optix Studio 1.6.3 and run in Emulator. I have found an example from NetLogic_CheatSheet/pages/trends.md at main · FactoryTalk-Optix/NetLogic_CheatSheet · GitHub to add a Y axis to a pen but I think the example is broken. I do not find the pen.YAxes.Add(yAxis); but I guess ...