List of Contributions

George

Contact Details

George


My Content

1 to 20 of 21 total
Posted By George Jun 19, 2023 05:38:00 AM
Found In Egroup: Advanced Software
\ view thread
EDIT: moved to Advanced Software community - PLEASE post FactoryTalk View SE related request directly in that community -FL In factorytalk view i exported some graphic displays from one project and imported them to another project, but i am getting a white box with red cross marks in the imported display. ...
Posted By George Jun 19, 2023 05:11:00 AM
Found In Egroup: Advanced Software
\ view thread
Thank You Fuzzylogic. I made a new project and imported the .sed file. That did the job. ------------------------------ George ------------------------------
Posted By George Jun 16, 2023 08:04:00 PM
Found In Egroup: Advanced Software
\ view thread
I only have the folder and sub folder arrangement for the saved project. It is a project from another computer. I dont have any MER file. ------------------------------ George ------------------------------
Posted By George Jun 16, 2023 07:02:00 AM
Found In Egroup: Advanced Software
\ view thread
EDIT: moved to Advanced Software community -FL I have factorytalk view SE software version 9.0 I need to open another factorytalk view saved project file. The saved file consists of a folder and many sub folders. There is no particular file to double click and open. (for example its an .acd file for ...
Posted By George Jun 14, 2023 02:22:00 AM
Found In Egroup: Automation Control
\ view thread
EDIT: moved to Advanced Software community -FL I am doing a project using studio 5000 and factorytalk view SE 9.0. I do not have any hardware with me to test the PLC program. In the factorytalk, i set up a server using factorylinx, and when i come to the communications setup, it is showing that ...
Posted By George Jun 13, 2023 01:51:56 AM
Found In Egroup: Automation Control
\ view thread
Thank you johnd_125. This answer helped me a lot. ------------------------------ George ------------------------------
Posted By George Jun 13, 2023 01:51:25 AM
Found In Egroup: Automation Control
\ view thread
Thank You Morley. Much appreciated. ------------------------------ George ------------------------------
Posted By George Jun 13, 2023 01:50:21 AM
Found In Egroup: Automation Control
\ view thread
Thank you Fuzzy Logic. I got the solution for this query. ------------------------------ George ------------------------------
Posted By George Jun 10, 2023 03:26:03 AM
Found In Egroup: Automation Control
\ view thread
Thank you. This helped me a lot. ------------------------------ George ------------------------------
Posted By George Jun 10, 2023 03:25:07 AM
Found In Egroup: Automation Control
\ view thread
Thank you Keith. ------------------------------ George ------------------------------
Posted By George Jun 10, 2023 03:16:43 AM
Found In Egroup: Automation Control
\ view thread
This digital tag had no error in the original program which I copied it from. I tried one thing. I deleted all other tags except this one alarm digital tag. Then i observed the same red color error in the original program. This means that deletion of a tag related to this caused the red error. ...
Posted By George Jun 10, 2023 03:13:03 AM
Found In Egroup: Automation Control
\ view thread
Thank you Daniel. This will help me a lot in the future. ------------------------------ George ------------------------------
Posted By George Jun 10, 2023 03:11:29 AM
Found In Egroup: Automation Control
\ view thread
Thanks for the support. ------------------------------ George ------------------------------
Posted By George Jun 09, 2023 04:23:00 AM
Found In Egroup: Automation Control
\ view thread
how can i download rstrainer for compactlogix and for controllogix. I tried the steps and i ambeing asked a serial number. How can i get the serial number. I have serial numbers of two RSlogix 5000 softwares I purchased. will that work? ------------------------------ George ---------------- ...
Posted By George Jun 07, 2023 04:22:00 AM
Found In Egroup: Automation Control
\ view thread
How do you find the maximum number of inputs and outputs(both analog and digital) a controller can handle. 1.Do you base it on the capacity tab in controller properties. If so how do you calculate the number of Inputs and outputs? 2. I am given a project. I have 50 DI, 42 DO, 5 AI and 3AO. ...
Posted By George Jun 07, 2023 01:54:00 AM
Found In Egroup: Automation Control
\ view thread
i am trying to understand an old program. i tried to cross reference some alarm group tags from an add on instruction, but it is linked to only the same add on instruction and nowhere else. How is the system for alarm groups tags. How to find out where they are linked besides the add on instruction ...
Posted By George Jun 07, 2023 01:49:00 AM
Found In Egroup: Automation Control
\ view thread
i am trying to copy one program and make an other program based on it in studio 5000. I created some alarm digital tags by copying from an older program and pasting it to the new program. but i am seeing a red error indication as shown in picture. whats the reason for the red error ------------ ...
Posted By George Jun 06, 2023 10:34:00 AM
Found In Egroup: Automation Control
\ view thread
I am a new programmer in studio 5000. I accidently created all the tags of a PLC program as controller tags. I recently leaned the concept of not to put all tags in controlle tags(i mean to save scan time and memory we have to put hardware and important tags in controller tags and rest in program tags). ...
Posted By George May 31, 2023 01:01:00 PM
Found In Egroup: Automation Control
\ view thread
I recently came across automation engineers using add on instructions already made by some one else. these add on instructions are used for example 1. module validation 2. interlocks 3. alarms etc my question is - is there any source on the internet where you can find these add on instructions already ...
Posted By George May 28, 2023 11:05:00 PM
Found In Egroup: Automation Control
\ view thread
I have addded a 16 bit DI card. i cant find the tags of the corresponding 16 bits in "controller tags". There are hundreds of tags in controller tags. 1. I want to find the tags for the corresponding bits if the DI card without manually searching it in the controller tags window. ------------------------------ ...