List of Contributions

PaulGallagher

Contact Details

PaulGallagher


My Content

1 to 20 of 50+ total
Posted By PaulGallagher Jul 23, 2026 09:39:19 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I get what you are saying. They would only be happy with the exact revision like 1.6.0.626 if it was installed with that then 1.6.0.625 or 1.6.0.627 would still not be accepted. That is why we ship the installation files with the machine.
Posted By PaulGallagher Jul 23, 2026 08:34:41 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Fuzzy, Thanks for the information, I feel the customer would have expected to be able to buy spare parts for something like 20 years. They are not happy about this. Basically as new builds are made they would need to keep spares for each type of panel instead of just one. It should always be possible ...
Posted By PaulGallagher Jul 23, 2026 03:52:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, A customer with validated machines that have version 1.6 installed has been told that pannels will only be supplied with version 1.7 in future. Will it be possible to down rev them to 1.6? Before we were able to go back a few revisions then up rev to the one we want. The customer will never ...
Posted By PaulGallagher Jun 19, 2026 06:51:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks Asemlucben, I added the group I in on the active directory, I had been trying this before but with the problems with the fully qualified name I had not completed it. After going back here it seems to accept the authority and make the change I was making with the signature. ...
Posted By PaulGallagher Jun 19, 2026 06:48:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have an update so hold of for a bit
Posted By PaulGallagher Jun 19, 2026 06:11:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I was having problems with the roles being assigned to the active direcgtory user. I have resolved this by using the fully qualified string when logging in that is DomainName/GroupName. For the signing in I am getting First user is not autherised mesage wihich is coming from the SignWorkflowHandler. ...
Posted By PaulGallagher Jun 18, 2026 05:58:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I am finding that the active directory user is logged in but there is a problem that was not there earlier where the user group has roles assigned to it but they are not working, this had been working and I am not sure at what point this stopped working but that is a seperate issue to the the audit signing ...
Posted By PaulGallagher Jun 18, 2026 04:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
There is also the auditdialogue box which uses local users so I think it will only pass local users.
Posted By PaulGallagher Jun 18, 2026 03:54:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks asemlucben, I change the combo box to a text box, I am getting this message now when I use my network credentials to sign, This does not happen when I use local users to log on instead. I changed the netlogix to reflect the change, I am wondering if wont work ...
Posted By PaulGallagher Jun 17, 2026 09:58:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, I have set up active directory and I can log in with credentials. I now need to add a audit trail. I have done this for local users and it is working but I have a drop down linked to the users in the model which are local. I need to change this so I can type in the user and hope that with ...
Posted By PaulGallagher May 07, 2026 05:12:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have a button to close it but that is only visible to the right user. The X is like on a web brower at the top right beside the minimise button. I did what CodeAssist said and it worked, I had full screen already and did not expect making always on top true to make any difference but it did. ...
Posted By PaulGallagher May 06, 2026 09:37:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
In my project I use static frame, it has a panel loader for other screens, it already is set to full screen this works for the emulator but on the runtime I see the X button. -------------------------------------------
Posted By PaulGallagher May 06, 2026 09:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Asemluchben, I deleted the user managment then put in a new one, the issues I was seeing are gone. Also the active directory user was not added to the list. As I only want local users everything seems fine now. Thanks -------------------------------------------
Posted By PaulGallagher May 06, 2026 07:55:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have a runtime, when it runs there is an x buton which means any user could close the application. I have an inbuilt button on the HMI, only one user can use the button. I need the HMI to occupy the full screen with no ability to close it. ------------------------------------------ ...
Posted By PaulGallagher Apr 28, 2026 10:07:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Asemlucben, Yes I agree but the user Paul.Gallagher and Paul.Gallagher@DomainName were added when I logged in using active directory and I do not want this to happen. That is why I am thinking I need to hide the users after my local variables. But if I want to create a new local variable ...
Posted By PaulGallagher Apr 28, 2026 09:14:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Asemlucben, Thanks for the feedback there. If you delete the retentativity database would any new users you added be gone? Would the users update and as design time after doing this and then you would have to save the files for validation purposes. Also as this is a runtime I am not sure what ...
Posted By PaulGallagher Apr 28, 2026 08:16:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
So the users are missing the one I was trying to delete, the error makes sense but the system seems not to work as expected as you can create but not delete, -------------------------------------------
Posted By PaulGallagher Apr 28, 2026 08:11:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
This might help, -------------------------------------------
Posted By PaulGallagher Apr 28, 2026 08:04:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have a few problems using the USER Managment. I removed the create and delete buttons as when I tried to delete a user it was not allowed. This was after just creating the user on an emulator. The program will be deployed to a wondows 11 enterprise server that uses active directory ...
Posted By PaulGallagher Mar 18, 2026 10:14:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I am using the, IdleTimeoutLogic script. The Idle logout time depends on the user. When I hard coded this using a Key Value converter this worked fine. For this project I need the time to be configurable by an admin user on the HMI. The Idle time logout uses the Duration type (000:00:00:000) ...