List of Contributions

Faisal

Contact Details

Faisal


My Content

1 to 5 of 5 total
Posted By Faisal Nov 29, 2025 11:12:00 AM
Found In Egroup: Automation Control
\ view thread
Philip Hamilton, I tried to optimize the CPU performance by adjusting the task periodic times-from 100 ms to 450 ms and from 200 ms to 350 ms. Before these changes, the CPU utilization was at 100%, and the entire system was hanging because some tasks were overlapping. I have attached a video(Task ...
Posted By Faisal Nov 27, 2025 10:22:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you, Philip Hamilton, for your response. I observed through the Task Monitor tool that my CPU usage was consistently at 100%, which was causing communication delays. I attempted to optimize the user tasks that were consuming the most resources by increasing the periodic task intervals from 100 ...
Posted By Faisal Nov 27, 2025 09:55:00 AM
Found In Egroup: Automation Control
\ view thread
I am currently encountering a critical issue with two MicroLogix 1400 PLC units. Over the past two days, both controllers have entered a fault state with Error Code 000BH, and the FAULT LED continues flashing. After clearing the fault and attempting to switch the controller to RUN mode, the PLC immediately ...
Posted By Faisal Nov 10, 2025 06:52:00 AM
Found In Egroup: Automation Control
\ view thread
When CLX operating in standalone (non-redundant) mode, the system performs normally-SCADA workstations respond quickly, and update rates are satisfactory. However, when redundancy is enabled, the SCADA update rates noticeably degrade, and intermittent communication hangs are observed across the network. ...