List of Contributions

Tan

Contact Details

Tan


My Content

1 to 20 of 50+ total
Posted By Tan Nov 06, 2025 06:44:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Fuzzy, yes the restart take longer once after the FTView version 15/16 is installed, in Windows 11 Pro. The software is smooth to use after restart, no impact on usage, but poor for user experience especially restart needed scenario. We are testing on Dell PC, DL-PROMAX-MT05, DELL/C PC ...
Posted By Tan Nov 06, 2025 04:03:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi all, I encountered an issue with FactoryTalk View Site Edition running on Windows 11 Pro. The following versions were tested: FTVSE v15 and v16. Both versions experience a delay of approximately 5 minutes showing the "Restarting" screen before the system actually restarts. Only version 14 does ...
Posted By Tan Jun 25, 2025 08:23:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Shane, thanks for the reply. Regarding this "The limitation will be the runtime device", can you help to elaborate on this? Currently I only sure that the runtime is depends on token, if more than 2 modbus TCP node, it will take 2 tokens. I have a coming scenario, which might need more than 60+ modbus ...
Posted By Tan Jun 23, 2025 08:18:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi all, Can anyone help to share documents regarding the maximum modbus tcp connector allowed for a FTOptix project file? Thank you.
Posted By Tan Apr 11, 2025 12:55:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks Shane for the great explanation. There are some much more to learn in FTOptix.
Posted By Tan Apr 10, 2025 08:39:02 AM
Found In Library: FactoryTalk Optix
Posted By Tan Apr 10, 2025 08:39:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
here is the testing application file
Posted By Tan Apr 10, 2025 08:36:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Shane, yes I am referring to this netlogic Session.User.BrowseName is return root user. I have attached a simple test user application, can you help to have a look? on runtime first startup, the netlogic first execution detect root because no user log in. After log in any user1/user with password ...
Posted By Tan Apr 09, 2025 09:30:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Shane, sorry to hijack this post but the question should be related. I have similar need to get the log in username in netlogic. Refer to sample project FeaturesDemo2 This code is working well in the sample project to log in username. However when I try to do the similar thing in my fresh ...
Posted By Tan Apr 03, 2025 05:20:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi All, I am referring to this part "Subscribe to new alarms and get notified at every Acknowledge or Confirm event": https://github.com/FactoryTalk-Optix/NetLogic_CheatSheet/blob/main/pages/alarming.md From the testing, I noticed FTOptix alarm state work in below sequence: Sequence 1 ...
Posted By Tan Mar 21, 2025 07:46:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi all, I would like to know is there any limitation or consideration if both FTOptix and FTView SE running their runtime client at same time and pointed to one AB PLC.
Posted By Tan Jan 08, 2025 07:57:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Shane, Thanks for the clear explanation. At the end I using below code to get value without displaying the tags at UI ushort Char11 = (ushort)Project.Current.GetVariable("CommDrivers/ModbusTCP3/Tags/ModbusTag1").RemoteRead();
Posted By Tan Jan 08, 2025 05:24:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi all, I noticed if the modbus tag is not put in Label and displayed at runtime, the modbus is actually no polling from slave, even though configuration is done. Below is my modbus TCP configuration This resulting the netlogic which refer to modbus tag is always ...
Posted By Tan Jan 06, 2025 07:30:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Yes! Using this path I can successfully bring the modbus tag value into Netlogic
Posted By Tan Jan 06, 2025 07:25:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
After some trial, I find out is the matter of register orientation, to get correct reading in int64, the 4 registers have to be arranged as 4004 join 4003 join 4002 join 4001 however when I tested it with expression, I still cannot get the result:
Posted By Tan Jan 06, 2025 04:39:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi all, one of my previous development in FTOptix 1.3.3.3 is always having an issue. The runtime client (workstation Windows 11) can be started and display properly, however after certain time, the client display will be disappeared from desktop view, including minimized task bar. It still running fine, ...
Posted By Tan Jan 06, 2025 12:24:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Shane, Thanks for the reply. I am not writing to the 4 registers, I am taking the 4 registers value from modbus station node, and would like to combine the 4 registers value into one single int64 variable. At moment, I have successfully convert some other devices which data spread across ...
Posted By Tan Jan 02, 2025 07:02:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi all, i am trying to poll modbus TCP from a powermeter and I have problem on putting the result into int64 modbus address / raw value in hex 4001 = 0000 4002 = 0004 4003 = A59C 4004 = 8920 this conversion is performed correctly using normal programmer calculator However ...
Posted By Tan Dec 06, 2024 12:49:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Shane, can you help to further explain how to use OptixPanel to print? 1. Do we need to install printer driver at OptixPanel Linux? If so, can you help to list out the step? 2. Is it using CUPS can print to printer? If so, how can I proceed to send opkg install cups to OptixPanel Linux? ...
Posted By Tan Jun 20, 2024 09:55:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
In version 1.4, is there anyway to lock the Netlogic file? Other than putting it under a panel.