List of Contributions

Butler

Contact Details

Butler


My Content

1 to 9 of 9 total
Posted By Butler Nov 18, 2025 09:03:04 AM
Found In Egroup: Automation Control
\ view thread
Just in case anyone came across this thread and wanted to know what the final outcome was. From what I have found, it is not possible to index through a tag array in the View Designer application. I have tried binding to a tag and creating an expression but neither work as when the project is verified ...
Posted By Butler Nov 12, 2025 08:22:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, Thank you for the suggestion. In the end I changed the view designer program so that the HMI user changes the value of HMI_Recipe_Select tag which is used within the logix software to copy the Recipe array value into a new Tag, HMI_Recipe_Display (same UDT data type). This can then be edited ...
Posted By Butler Nov 11, 2025 04:15:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, I've used this technique in Studio 5000 to dynamically change the array value of a tag that I am viewing. I am trying to adopt the same method for use in my View Designer project. I have a UDT with various data types to store recipe parameters, the controller tag is Recipes[300]. I also ...
Posted By Butler Mar 06, 2025 05:03:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, Updating the firmware has worked a treat! I used the flash plus program and it turned out that the firmware revision on the device was actually 6.013 even though the sticker on the side of the device said 7.011. I updated the firmware to the latest revision, 7.015, rebooted the device ...
Posted By Butler Mar 05, 2025 07:10:00 AM
Found In Egroup: Automation Control
\ view thread
Hi FL, No I haven't tried that, I'll try that tomorrow and let you know if it works as the device is currently at my home so I can test the remote connection of a Tosibox!!! Thanks, Luke
Posted By Butler Mar 05, 2025 02:28:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, Thanks for the response, the firmware of the Point IO device is 7.011. I know from reading some literature that if the firmware version is lower than 2.001 the web browser feature has to be enabled.
Posted By Butler Mar 04, 2025 09:35:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, Usually, I can connect a #PointIO module to my PC once I've set the dials to a value between 1-255 and have my PC network settings on the same range (192.168.1.xxx). I check this by pinging the device before opening the web browser and typing in the IP address. Normally I would write the ...
Posted By Butler Jun 04, 2024 04:18:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, Thank you both for this discussion, I am just looking into a similar application and this thread has been very informative. I just wanted to confirm the solution to this issue if using a safe edge in combination with the 5069-IB8S safety input card would be to set the RPI the standard DC output ...