List of Contributions

Lazarski

Contact Details

Lazarski


My Content

1 to 13 of 13 total
Posted By Lazarski Jun 09, 2026 01:28:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Unfortunately that amount of process of elimination doesn't work in my scenario. The report generates fine on my machine. I will then commit and push changes on the project to our bitbucket repository. Then if I clone the repository and open the cloned repo, the report generation fails with ...
Posted By Lazarski Jun 05, 2026 06:59:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
So there's no way for me to dig deeper into log files or the Optix backend and see what the issue is? It's surely not a file IO permissions issue since I even tried to move the project into a C/users/public folder. This issue seemingly happens whenever I clone the project from a repo, oddly enough
Posted By Lazarski Jun 04, 2026 05:59:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Is there a way to view more information on some error codes that pop up but don't specify much detail? For example, this error code is all that is shown after my PDF report fails to generate. The runtime logs offer no more information than this and I need to try and figure out a fix. ...
Posted By Lazarski May 13, 2026 09:17:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
In the Optix github repository there's also a method that allows you to create a web server which any computer can connect to and download files from https://github.com/FactoryTalk-Optix/Optix_Sample_DownloadFileToWebClient -------------------------------------------
Posted By Lazarski May 08, 2026 07:21:00 AM
Found In Egroup: Advanced Software
\ view thread
That is what we noticed -- trying this on a PVP7 Standard completely does not work. The latest test case was using a PVP7 Performance Ser.B. I believe the currently loaded firmware is 12.108 When clicking the web browser object, I was able to access the Edge pop up window. If firmware ...
Posted By Lazarski May 07, 2026 02:41:00 PM
Found In Egroup: Advanced Software
\ view thread
Yes, each component has been tested and works independently. Optix web engine in a computer browser, FT View web browser to an accessible web page, etc There are specifically issues with the ME web browser accessing an Optix web engine -------------------------------------------
Posted By Lazarski May 07, 2026 02:01:00 PM
Found In Egroup: Advanced Software
\ view thread
Sorry for not providing sufficient detail in the original post. FT Optix runtimes through the web presentation engine are not natively supported by FTView ME web browser objects. Navigating to a web presentation engine in a FTView ME panel results in a blank screen. This seems ...
Posted By Lazarski May 06, 2026 07:12:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, Has anyone had any luck getting a FTView ME panel to connect to a FTOptix web presentation runtime via the ActiveX web browser objects? I've heard there's possibility of getting that to work, and in testing it I can sort of get it to work. I haven't been able to get the Optix runtime ...
Posted By Lazarski Apr 22, 2026 10:41:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I can't seem to get the built in "duration" object to work with Stylesheets. The default selected stylesheet is of the type Input Box Styles, however, if I make a new input box style and set the Duration object to use that, it doesn't do anything. Is there something I'm missing, because it doesn't seem ...
Posted By Lazarski Apr 03, 2026 08:43:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
The syntax of <> works, thanks! -------------------------------------------
Posted By Lazarski Apr 02, 2026 04:43:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I tried a few permutations of the syntax including IS NOT / NOT IS which didn't work, albeit I did not try the "IS LIKE" syntax. Is a NuGet library the recommended way to interface with the embedded databases? -------------------------------------------
Posted By Lazarski Apr 02, 2026 09:13:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I suspect there might be some weird things happening under the hood of the query parser in FTOptix and am looking for some assistance. I understand FTOptix only uses a subset of SQLite commands, but this doesn't seem right. The database table Recipes has a column Name of type string, and ...
Posted By Lazarski Mar 26, 2026 12:59:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Is there a location for Optix bug reports -------------------------------------------