List of Contributions

Shawn Tierney

Contact Details

Shawn Tierney


My Content

1 to 20 of 41 total
Posted By Shawn Tierney Mar 30, 2023 03:47:00 PM
Found In Egroup: Advanced Software
\ view thread
Do you see a help menu in FTView - all my Rockwell Software has Help menus, and help can also be accessed using F1. I believe the "online manuals" are also installed by default, as well as linked to under the help menu? Update: Yeah, I was right: DON'T Discount the HELP - Contents, occasionally ...
Posted By Shawn Tierney Mar 15, 2023 04:53:00 PM
Found In Egroup: Installation & Activation
\ view thread
Are you sure you can have two minor revs installed on the same PC? 32.01.00 & 32.04.00? I've never heard of this being supported? ------------------------------ Shawn Tierney The Automation Guy and author of The Automation Blog Host of The Automation Show, Podcast, Minute, and Morning Show ...
Posted By Shawn Tierney Mar 09, 2023 04:37:00 PM
Found In Egroup: Automation Control
\ view thread
Great question, First, the 5370 line (L1xER, L2xER, and L3xER) CompactLogix controllers had a supercap inplace of a battery. That said, with any A-B PLC I can think of, when power is lost the controller has to come out of Run mode, and you should get a First Scan/First Pass bit turning 1 for ...
Posted By Shawn Tierney Mar 08, 2023 05:19:00 PM
Found In Egroup: Advanced Software
\ view thread
We use to do this A LOT in RSView32 because the VBA was server side. In ViewSE the VBA is Client side, so not so good on a client-server system since the text files would be created on the clients (but it sounds like you have a single station system, so they are the same.) Honestly, imo it would ...
Posted By Shawn Tierney Mar 06, 2023 04:56:00 PM
Found In Egroup: Automation Control
\ view thread
To add to what the guys already said, the first time most of us ran into this exact issue we didn't realize the patch roll-up not only updated the software but also sometimes updates the ActiveX's too, thus resulting in this error. ------------------------------ Shawn Tierney The Automation Guy ...
Posted By Shawn Tierney Mar 06, 2023 04:46:00 PM
Found In Egroup: Automation Control
\ view thread
Hey Mike, Just going to share some thoughts here that might help. So this is a common request - OEMs want one file for all the HMIs, except that file has to be "a little" different for each HMI. In your case, it's the current display screen / remote display screen control via Global Connections ...
Posted By Shawn Tierney Mar 01, 2023 05:21:00 PM
Found In Egroup: Advanced Software
\ view thread
So glad you liked it @fuzzy logic I have quit a bit of nostalgia for the original RSView. I use to really struggle with ControlView for Dos, so I was determined to become an expert with WinView. Funny thing is, while in an in-person WinView class at the old Icom building in West Allis, the ControlView ...
Posted By Shawn Tierney Mar 01, 2023 12:28:00 PM
Found In Egroup: Automation Control
\ view thread
I'm very interested in learning why the IP Address did not update as well, seeing as it's a 5370...? BTW - Unlike some Siemens models, with A-B you can use any SD Card (of a supported memory size,) not the only one you have from Rockwell :-) ------------------------------ Shawn Tierney The ...
Posted By Shawn Tierney Feb 28, 2023 05:17:07 PM
Found In Library: Advanced Software
Posted By Shawn Tierney Feb 28, 2023 05:17:00 PM
Found In Egroup: Advanced Software
\ view thread
You're very welcome! If the product was new I'd lobby for an update to this feature (well, I'd still like to see updates,) but as I mentioned it's been like this since the original RSView came out in... 1995, so most of us are just use to it. Best wishes, Shawn PS - I'll try to attach the data sheet ...
Posted By Shawn Tierney Feb 28, 2023 05:06:00 PM
Found In Egroup: Advanced Software
\ view thread
Perfect! ------------------------------ Shawn Tierney The Automation Guy and author of The Automation Blog Host of The Automation Show, Podcast, Minute, and Morning Show ------------------------------
Posted By Shawn Tierney Feb 28, 2023 04:46:00 PM
Found In Egroup: Automation Control
\ view thread
I don't work for Rockwell, but I have been using their PLCs for a little while and can say that as far as I know (going all the way back to the early 90's,) you have never been able to do this with any A-B PLC... well, aside from burning EEPROMS and old tech like that. I also can confirm what you ...
Posted By Shawn Tierney Feb 28, 2023 06:04:00 AM
Found In Egroup: Advanced Software
\ view thread
Personally, I've don't ever remember finding a way to get rid of, or customizing, the border of the Numeric or String Inputs. If someone else has please share. You should be able to make your Numeric and String display objects have a similar look by giving them have a transparent background and grouping ...
Posted By Shawn Tierney Feb 27, 2023 03:12:00 PM
Found In Egroup: Automation Control
\ view thread
I'd be interested if you figure this out - I've always sent the info over to a tag, then used an SSV in the destination controller. ------------------------------ Shawn Tierney The Automation Guy and author of The Automation Blog Host of The Automation Show, Podcast, Minute, and Morning Show ...
Posted By Shawn Tierney Feb 24, 2023 02:10:00 PM
Found In Egroup: Advanced Software
\ view thread
In FTViewSE (and RSView32) I believe you will find Numeric and String Input settings under the Display's Settings (where they are set once for the entire display.) It's a little limiting, but there are ways to get around it... ------------------------------ Shawn Tierney The Automation Guy and author ...
Posted By Shawn Tierney Feb 21, 2023 05:08:00 PM
Found In Egroup: Advanced Software
\ view thread
Yes! I've done it a thousand times :-) But you must insure the format doesn't change. Compare the old file to the new and you'll probaby find something missing in the new. To avoid that, I always create a test tag of each type, and then in Excel I duplicate those. Also be careful with Excel when ...
Posted By Shawn Tierney Feb 20, 2023 03:40:00 PM
Found In Egroup: Automation Control
\ view thread
Great news Kam! Glad you got it working :-) PS - and thank you for your kind words! ------------------------------ Shawn Tierney The Automation Guy and author of The Automation Blog Host of The Automation Show, Podcast, Minute, and Morning Show ------------------------------
Posted By Shawn Tierney Feb 20, 2023 03:37:00 PM
Found In Egroup: Legacy
\ view thread
Ok, so it's not loading from non-volatile... in that case the next likely scenarios are: (1) It's setup for bootp-dhcp, and you haven't disable it / changed it to static or (2) the IP address is being changed via the code (likely via an SSV.) Shawn ------------------------------ ...
Posted By Shawn Tierney Feb 20, 2023 03:32:00 PM
Found In Egroup: Legacy
\ view thread
Hi Jan, Great question. The short answer is no, but A-B PLCs/PACs have to be in program mode to save to non-volatile, so it's typically not an issue BUT it can be depending on how the system is programmed (we could talk for hours just about this :-) Sincerely, Shawn ------ ...
Posted By Shawn Tierney Feb 17, 2023 04:24:00 PM
Found In Egroup: Automation Control
\ view thread
Hey Kam, Yeah CCW is a little different then FTME, but the basic idea is the same: In each screen's properties there is a screen number In Tags you will find a Global Connection called "current screen number" Write a non-zero number to a tag you assign there, and that will ...