List of Contributions

Michael Demers

Contact Details

Michael Demers


My Content

1 to 6 of 6 total
Posted By Michael Demers Apr 29, 2024 12:30:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello, I added an FT historian SE license 'FHIST.1000' in Factorytalk Activation Manager. However, I am not able to see it in FT administration console to be able to assign it to my historian server. I have FT Historian SE V6.00 which has already assigned an FHSE.250 license (the basic one) and another ...
Posted By Michael Demers Oct 05, 2023 01:58:14 PM
Found In Egroup: Advanced Software
\ view thread
Thank you for all the information and the responses. I actually have FT view SE which limits me to 20 Data Logs who's running at the same time. I read on the web that 'FT Transaction manager' could solve my problem. It will do the same job as a Data log. I would like to know if there is also a limit ...
Posted By Michael Demers Oct 04, 2023 02:38:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello, I would like to know if it is possible to increase the number of active Data logs at the same time. I have to create several reports (more than 20 reports) by SQL which each depend on a datalog. I would like to know if it is possible to increase the number of active data logs at the same time ...
Posted By Michael Demers May 02, 2023 08:39:42 AM
Found In Egroup: Advanced Software
\ view thread
Is the Exception Max Time work only when Location 3 = 1 ? Because right now i have a point for each tag change (Location 3 = 0) but not every 6 hours. ------------------------------ Michael Demers ------------------------------
Posted By Michael Demers May 01, 2023 10:15:00 AM
Found In Egroup: Advanced Software
\ view thread
I would like to create historian points each time a Tag changes value as well as every 6 hours. (Ex: if the tag value change at 13h17, I want the tag value at 00h00, 06h00, 12h00, 13h17, 18h00). Can you help me to find the right combination of parameters for this. ------------------------------ ...
Posted By Michael Demers Sep 16, 2022 08:50:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, my project is to create some reports by microsoft visual studio by using a database from FT historian. I would like to know if it's possible to create a communication link between these two programs without going through SQL server? If the answer is no, is it possible to create a link between ...