List of Contributions

Fox

Contact Details

Fox


My Content

1 to 20 of 50+ total
Posted By Fox Feb 02, 2026 10:06:34 AM
Found In Egroup: Automation Control
\ view thread
Thanks for the tag Shane! Hey Retzlaff, There's a lot to unpack here. What's the speed of the conveyor? What sensors are you currently using? do these numbered carriers have any kind of RFID or anything else other then text for tracking the carriers? There's lots of great options, but i need more ...
Posted By Fox Jan 22, 2026 06:34:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi all, I'm looking to understand how others are managing versioning, lifecycle, and compatibility across reusable controls libraries-specifically when PLC Add-On Instructions (AOIs) and HMI visual components are developed and maintained together. The problem we're trying to solve At a company ...
Posted By Fox Jan 22, 2026 06:16:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I'm wondering if anyone has had any consistant success in working with IT departments of large customers that would allow an Optix panel to communicate to the internet over there plant network. Security wise it seems like its in a good position with outbound only connections, but getting buy in from ...
Posted By Fox Nov 03, 2025 06:57:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Flareux, I would bring the entire tag in as an alias or node pointer (as opposed to a node id as a variable) into your widget.. then just reference that alias or node pointer anywhere inside your widget. You shouldn’t need the @value. -------------------------------------------
Posted By Fox Nov 02, 2025 09:15:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Souman, have you tried opening a backup or previous commit of your project? -------------------------------------------
Posted By Fox Nov 02, 2025 01:03:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Brian, I think if I understand right, you just want MSB * 65536 + LSB ? If so, an expression evaluator will do the job. when you go to add a dynamic link to a label, click on the advanced tab, select + and select expression evaluator. enter (0) * 65536 + (1) Two ...
Posted By Fox Nov 01, 2025 11:57:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Kataray, As Blake said, Welcome to Optix! To get started, there's a Fiix library for Optix that may just get you what your looking for. Here's a link to the documentation. Fiix Library For Optix However, if you want to roll your own... Combo Box The model for a combo ...
Posted By Fox Oct 20, 2025 07:22:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I assume this is for a discrete input or output card? Should be doable, but it will require some Netlogic code. I would suggest starting by examining the structure of the tag in Netlogic (set a breakpoint after it reads the tag, then hover over it to explore the structure). Those extended tag properties ...
Posted By Fox Oct 17, 2025 09:12:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Woops! We have an error in the expression evaluator. Make those a double equals and it should fix it. -------------------------------------------
Posted By Fox Oct 17, 2025 08:20:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
That model variable that you created, set its value to 3 in the design environment. Then it will default to that on startup, and the option button will be checked. -------------------------------------------
Posted By Fox Oct 16, 2025 11:36:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
One way you could find this is to search for it. If you right click on a folder, you have the option to search for that problem object. -------------------------------------------
Posted By Fox Oct 16, 2025 11:28:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Scott, Sure thing, So for this you can setup a dymanic link for the checked property. Click on the advanced tab, and select an expression evaluator. In this first one we'll look for the value of the model variable to be equal to 3. Then setup the second one the same way, comparing it to 325 ...
Posted By Fox Oct 16, 2025 10:26:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Angelo, Great question, and welcome To Engage! Quickest option: put the engineering unit to the right of the input as a Label (often inside a horizontal layout, so it stays aligned) with either a SpinBox or TextBox. Why not inside the field? The SpinBox only accepts numeric input, ...
Posted By Fox Oct 15, 2025 09:03:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Palic, As it turns out, The Optix help documentation has a full tutorial to guide you through this process step by step. To get started, you can go to the help file in Optix and search for "OPC UA Tutorial". This should be a good base to help you get your bearings! ------ ...
Posted By Fox Oct 15, 2025 07:07:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Kataray, Just to complete the thread for anyone else running across your issue, what's this the error message you were getting? Coincidentally, we had a user struggling with this for a few days and was working with RA tech support on it. In Optix, when you clicked gethub and authenticate, ...
Posted By Fox Oct 13, 2025 07:16:20 AM
Found In Egroup: Automation Control
\ view thread
Hey Finnegan, Welcome to Engage! I can only speak for the FT Optix training, but if you're interested in learning about next-gen HMI development, the Rockwell team did a fantastic job with Optix. It goes a lot further then what you see at the Automation Fair and really dives into the details and ...
Posted By Fox Oct 12, 2025 11:00:00 PM
Found In Egroup: Advanced Software
\ view thread
Hey Michael, Not an Emulate/FT Linx incompatibility. The mode changes you see (Power Up → Remote Program) happen when Studio 5000's programming path engages (Who Active / Download). The FT Linx data server won't change the controller/emulator mode-so those observations are normal. View SE uses FactoryTalk ...
Posted By Fox Oct 12, 2025 07:13:00 PM
Found In Egroup: Networks
\ view thread
Hey Xavier, Currently FT Remote Access does not support a way to automatically run and connect to a VPN on startup. For something like that I would suggest a NAT switch for connecting to the control network from the plant network. Then you could connect to the plant VPN remotely. Some corporate VPN's ...
Posted By Fox Oct 12, 2025 06:02:38 PM
Found In Egroup: Emulate3D Software
\ view thread
Hey Cannon! I just ran across your question and this type of stuff is intresting to me. It falls into that catagory of "automating the automation" which i'm a big proponent of. I'm not currently using Emulate 3D but I've been through the getting started boot camp a while ago and was asking questions ...
Posted By Fox Oct 11, 2025 03:03:00 PM
Found In Egroup: Advanced Software
\ view thread
Hey Perilla, I was recently playing around with objects in the library and noticed a few things that might be relevent to your issue. When you copy a widget into the library, its already including any nessessary data types with it. When you copy that widget back out of the library to a new project, ...