List of Contributions

Chris T

Contact Details

Chris T


My Content

1 to 20 of 21 total
Posted By Chris T Jul 22, 2025 01:43:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, So recently we had some issues with RPI's going over the time-out limit on CIP-Safety communications for external devices, specifically from one supplier. CPU Safety task time would be set to 20ms and standard time-out value would be 180ms. Now in some setups these times would go upwards to ...
Posted By Chris T Jul 08, 2025 12:26:00 AM
Found In Egroup: Advanced Software
\ view thread
To add on to this, and maybe help others a bit. We ended up removing our 'main' NetLogic. And moved all scripts to their respective panels. Only activating the required scripts (even the asynchronous tasks) when the panel is opened, closing/stopping when switching between panels. This has resulted ...
Posted By Chris T Jun 24, 2025 07:47:00 AM
Found In Egroup: Advanced Software
\ view thread
Okay, we found the 2nd NetLogic, it was nested in the MainPanelLoader. We will investigate further into seeing what is using so much CPU. Many thanks for your help.
Posted By Chris T Jun 24, 2025 05:24:00 AM
Found In Egroup: Advanced Software
\ view thread
Thanks a lot for your support so far. It has been very insightful already. We will have a look at the points you mentioned. One I am not sure we understand. There is mention that we have 2 Netlogics, however we have only one to our current knowledge. We have one main Netlogic, which runs ...
Posted By Chris T Jun 24, 2025 03:40:00 AM
Found In Egroup: Advanced Software
\ view thread
Please see attached file. Which parts would we have to look at in order to determine loading times or other bottlenecks? We have seen one message where it shows that a task is running too long. EDIT: There was only one log-file of today, so I am unsure what you mean by the 3 log-files.
Posted By Chris T Jun 24, 2025 03:39:51 AM
Found In Library: Advanced Software
Posted By Chris T Jun 24, 2025 02:53:00 AM
Found In Egroup: Advanced Software
\ view thread
Above the main overview. Goal of the panel is to show a dashboard with production values. It's built up of a MainpanelLoader and 11 panels that can be switched between. The main overview is (I assume) the most taxing page in terms of CPU. The sideways graph shows production state of the last 24 hours, ...
Posted By Chris T Jun 24, 2025 02:32:00 AM
Found In Egroup: Advanced Software
\ view thread
Thank you for this question! I found out that opening that in notepad actually contains quite some interesting data. The .optix file is attached. EDIT: Turns out the .optix format was not allowed... Is this the info you are looking for? If not, please let me know which section of the file you ...
Posted By Chris T Jun 23, 2025 09:09:00 AM
Found In Egroup: Advanced Software
\ view thread
Going up in versions is currently not feasible, as it's already running in the factory with no internet access at this moment. We haven't checked the panel firmware for the same reason (more or less)... The problem we are seeing is that it feels extremely sluggish at times, specifically notable when ...
Posted By Chris T Jun 23, 2025 08:34:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, Currently we have a Panel running at a customer with FactoryTalk Optix 1.6.0.132. It's running on a panel with the 2.2Ghz CPU and 4GB of 2133Mhz RAM. The FactoryTalk Optix Runtime application is using atleast 45% of CPU power by default. Which feels like an extremely high amount for us. ...
Posted By Chris T May 28, 2025 06:53:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Dear Vincent, That was the missing link for me! I couldn't find such an example yet. Many thanks for this insight. Regards,ChrisT
Posted By Chris T May 28, 2025 05:15:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Dear Vincent, Thanks for your reply. The manual you refer to clearly states 'MSG Access Only' for that attribute. So I do not fully understand which 'get' you are referring to? And a GSV does not show this parameter directly in the options. Regards ChrisT
Posted By Chris T May 28, 2025 01:38:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, We have an installation where we are using a Kinetix 5500 (Firmware 7.013) 2198-H025-ERS. With a VPL-B0753M-P motor. Connected to a 1756-L82ES (FW 33.11) controller. We would like to read the cumulative energy usage of the drive (or any energy usage tag available). However I cannot find ...
Posted By Chris T Feb 20, 2024 06:57:00 AM
Found In Egroup: Automation Control
\ view thread
Hello Philip, I think these checks cover what we want. And I agree we can use the I/O Led status to trigger these checks, however I expect that we will continuously or periodically do the checks with the GSVs. Regardless, thanks for your advise.
Posted By Chris T Feb 14, 2024 12:50:00 AM
Found In Egroup: Automation Control
\ view thread
Hey Philip, Thanks for the response. I was expecting this already yes. So just checking the EntryStatus is not enough. Now if I understand all correctly, then checking if the FaultCode of a module is anything other than 16#0000 (0) should give the desired result? And is this actually the best ...
Posted By Chris T Feb 13, 2024 06:13:00 AM
Found In Egroup: Automation Control
\ view thread
Hello all, There are multiple ways to check statuses for remote IO modules. Specifically for the 1734-AENTR / 1734-AENT /1734-IB4 1734-OB4 /1734-IB8S / 1734-OB8S which we use often within the company. Now currently there's about 3 different ways we check remote IO status. For the head ...
Posted By Chris T Nov 01, 2022 02:09:00 AM
Found In Egroup: Automation Control
\ view thread
I've read the ACM/LibraryDesigner manual (partially). But for the remainder I have just started working with it, progressively learning more and finding new features. I can say that this takes the longest amount of time to learn, atleast I think so. If you have standard pieces of software, that are ...
Posted By Chris T Oct 31, 2022 09:03:00 AM
Found In Egroup: Automation Control
\ view thread
Great to know we're not alone! I understand ACM is quite new for a lot of users as far as I have been able to find. However at my company we are running paid projects with it. This issue is only a small hiccup, but it's just annoying to have to go through an L5X file and fix about 80 modules. Still ...
Posted By Chris T Oct 31, 2022 01:53:00 AM
Found In Egroup: Automation Control
\ view thread
Thanks for your response. I do understand your point and I will try to get in touch with our RA sales person. However, I cannot fully understand why this function is not implemented from the start. I can't imagine nobody else is having this issue. Neither can I imagine that RA decided to skip this ...
Posted By Chris T Oct 28, 2022 04:26:00 AM
Found In Egroup: Automation Control
\ view thread
As an addition, the Controller Preview window in Application Code Manager does show the devices are connected to the A1 port of the controller, as seen in the image. However when opening the generated L5X file with studio 5000 the ParentModPortId is not working. ------------------------------ Chris ...