|
Hello all, I have a Kinetix 5700 (2198-D020-ers3 - Rev 14.001). Both axis' of the module are connected to identical motors (Linmot P10-70 motors). With the motors/drives powered on and at idle, one axis pulls 5% current and the other is pulling 35% current. Both motors are horizontal axis. The issue ...
|