List of Contributions

Enrique

Contact Details

Enrique


My Content

1 to 18 of 18 total
Posted By Enrique Oct 01, 2025 07:58:36 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello GAAM, We can send the encoder speed and position with Datalinks using EtherNet/IP network, but the data transfer will be much slower. SynchLink and T-Link data transfer is 125 usec and Datalinks is 2 msec (using min RPI allowed). We cannot guarantee it will be possible to do the application ...
Posted By Enrique Sep 30, 2025 02:43:23 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello GAAM, Tlink is not compatible with Synchlink. So you cannot migrate only one of the existing PowerFlex 700S drives to PowerFlex 755TS. It's necessary to replace both drives. The transmitter 700S drive is sending encoder 0 speed and position to the receiver 700S drive. With the PF755TS using ...
Posted By Enrique Jul 11, 2025 03:47:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Dobson, The PowerFlex 755 drives with firmware v20.003 have a new main control board (Series B) that requires firmware v20 min. So you can not flash these drives to v14. I suggest to install the new AOP v16.03 that support 755 drives v20. Best Regards ------ ...
Posted By Enrique Oct 02, 2024 01:43:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Kang, There are two parameter in the PowerFlex 525 that can help to keep the drive running during short term power sag. Set A548 [Power Loss Mode] to 1 "Decel" . Drive decelerates and attempts to keep the DC bus voltage above the undervoltage level. Set A549 [Half Bus Enable] ...
Posted By Enrique Aug 07, 2024 02:05:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
You can use two different deceleration ramps using decel time 1 (537) and decel time 2 (538) . You can switch from decel 1 to decel 2 with a digital input (DI Decel 2 - param 180) or by network . ------------------------------ Enrique Fabregas EMEA Commercial Project Engineer Rockwell Automation ...
Posted By Enrique Jul 01, 2024 02:02:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Adam, You can use Drive Explorer/DriveExecutive/CCW software packages to determine the PowerFlex Drive's Host Serial number from the main control board or the power board test. But this is an internal serial number that does not reflect the real Serial Number that is printed on drive nameplate. ...
Posted By Enrique May 09, 2024 07:49:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
PowerFlex 4 AC drives 200...240VC 1-phase (22A-Axxx) or 3-phase (22A-Bxxx) have a voltage range of 180..265V. There is no problem to work at 240V. ------------------------------ Enrique Fabregas EMEA Commercial Project Engineer Rockwell Automation ✔ Please Like the replies that you ...
Posted By Enrique May 09, 2024 01:24:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Hasak, By default the bus regulation in the PowerFlex 4 drive is enabled. This feature can extend the deceleration ramp if the bus voltage rises. Set parameter A117 [Bus Reg Mode] to 0 "Disabled" and test. Regards, ------------------------------ Enrique Fabregas EMEA Commercial ...
Posted By Enrique Apr 18, 2024 06:26:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello ZLG, This technote can help you : https://rockwellautomation.custhelp.com/app/answers/answer_view/a_id/491122/loc/en_US#__highlight Best Regards ------------------------------ Enrique Fabregas EMEA Commercial Project Engineer Rockwell Automation ✔ Please Like the replies ...
Posted By Enrique Apr 16, 2024 10:10:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I saw this fault in fan applications or high inertia loads because the bus voltage regulation is active and the drive can not follow the programmed deceleration. If the deceleration time is not critical for the application, I suggest to ignore this fault in parameter 0:409[Dec Inhibit Actn]. Best ...
Posted By Enrique Apr 16, 2024 09:59:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello J_Sanborn, You can limit the output current in the PF755 drive by writing in the parameter 0:422[Current Limit 1]. Value is in Amps. Best Regards ------------------------------ Enrique Fabregas EMEA Commercial Project Engineer Rockwell Automation ✔ Please Like ...
Posted By Enrique Mar 21, 2024 03:24:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Mike, You should verify the setup in the drive is according publication PFLEX-AT002 , PowerFlex 753/755 Parameter Settings for Use with Sine-wave Filters. (https://literature.rockwellautomation.com/idc/groups/literature/documents/at/pflex-at002_-en-p.pdf) Regards Enrique ...
Posted By Enrique Feb 06, 2024 05:15:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, While the drive is stopping, the Active bit is High and you are forcing the Stop bit to High. In this situation, the drive changes to Stop Asserted state (you are actively giving a stop command) and the ready bit goes to Low. You can see the Stop Asserted message on the HIM. When the ...
Posted By Enrique Feb 01, 2024 03:44:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Leebehzite, If you want to use a fixed IP address, you have to set parameter C128[Net Addr Sel] to Parameters and set the IP Address and Subnet Mask in parameters C129 to C136. Setting a Gateway Address is optional. After changing any of these parameters, you have to cycle power to the drive ...
Posted By Enrique Jan 29, 2024 01:50:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Rozoy , Parameter 951[Last Fault Code] shows fault codes only. Parameters 959[Alarm Status A] and 960[Alarm Status B] indicate the occurrence of conditions that have been configured as alarms. Best Regards. Enrique ------------------------------ Enrique Fabregas ...
Posted By Enrique Jan 24, 2024 03:10:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Ali , You should set parameter 545[Spd Ref A Sel] to Port0:Port 6 Reference Best Regards Enrique ------------------------------ Enrique Fabregas EMEA Commercial Project Engineer Rockwell Automation ------------------------------
Posted By Enrique Jan 22, 2024 02:26:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Gian, The 20G11NC085JA0NNNNN (PowerFlex 755) is 45Kw 85A Normal Duty and 37Kw 72A Heavy Duty. The first is to check the motor NP data. If you have an inclination of -17º could be necessary to add a brake resistor due to regeneration. The drive has an internal brake chopper. ...
Posted By Enrique Jan 18, 2024 06:09:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Yes, you should enter the correct number of motor poles , rpm and frequency. If you don't know one of this parameters you can use this formula: Frequency = (Poles x Ns) / 120 (Ns= synchronous speed) ------------------------------ Enrique Fabregas EMEA Project Commercial Engineer ...