|
Hello. May I ask you for one information about status data from Powerflex 525. We setup RPm according nameplate of motor to 1440 rpm. But when we start FD and run at 50Hz/100%. Actual value of RPM P15 Output RPM is 1500 RPM. Location is Europe, so the value max. herts is set up to 50Hz. ...
|