List of Contributions

Usamah Riaz

Contact Details

Usamah Riaz


My Content

1 to 5 of 5 total
Posted By Usamah Riaz Apr 26, 2024 08:26:56 AM
Found In Egroup: Automation Control
\ view thread
The card seems fast as the minimum filter time i see in the options from Off to On and On to Off is 0 micro seconds. If that is the case and if i go with formula for frequency F=1/T, then F seems to be infinite. Can it mean that the IB16 card input won't miss pulses of any frequency? ------------------------------ ...
Posted By Usamah Riaz Apr 26, 2024 04:36:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, I am using 5069-IB16 for Digital inputs. I also need to wire a few high speed inputs to the same card as I dont have high speed counter. What is the maximum frequency of pulses my card can detect considering that the minimum filter time i can set on 5069-IB16 is 0 micro second. ------- ...
Posted By Usamah Riaz Mar 15, 2024 11:59:00 PM
Found In Egroup: Installation & Activation
\ view thread
Hi everyone, I am trying to setup FTView SE V13 on my system which is an Intel Xeon W2123 Machine @ 3.6Ghz with a RAM of 16GB. It has been more than 12 hours and the setup is stuck at 64%. The setup file is on a usb. I tried the same after copying the setup on the system desktop but the result is still ...
Posted By Usamah Riaz Feb 02, 2024 11:16:00 PM
Found In Egroup: Automation Control
\ view thread
I wish to power cycle the MICRO820 controller using the CCW software from the tags created instead from removing the power. Please advise. EDIT: moved to Automation Control -FL
Posted By Usamah Riaz Nov 23, 2023 08:55:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi there. I am using CCW and FTView SE V13. I am connected to the controler Micro 820 through OPEN VPN. I can see the controllers thorugh ETHIP in Rslinx Classic and CCW Browser, but when i open communication setup in FTLinx to assign a topic to the controller, it doesnt show any connected devices except ...