List of Contributions

AZ Territory

Contact Details

AZ Territory


My Content

1 to 3 of 3 total
Posted By AZ Territory Jul 14, 2023 11:52:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Has anyone done it? Can anyone tell me how to do it? I have a reference card for the 525 and have done it a few different times in other buildings. In this building, which is much older, we have PF 40's and they are quite a bit different so I'm hesitant to use the same method. I'm the only ...
Posted By AZ Territory Jan 17, 2023 08:59:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I think I figured it out. For some reason there's a splitter plugged into the comms port on the bottom of the drive that turns 1 ethernet port into 2. Previously, when I plugged 1 HIM into the port labeled "Master" I was getting the setup only menu as shown in the pics. Thankfully I have 2 HIM devices ...
Posted By AZ Territory Jan 17, 2023 06:23:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Does anyone know if this is possible? Trying to replace a drive and am not able to pull up Copycat on the HIM device. It connects with an ethernet cable as opposed to having a slot on the front of the drive, but it's only allowing me to view a setup menu. It is giving me the message "Existing Master: ...