List of Contributions

resistor

Contact Details

resistor


My Content

1 to 5 of 5 total
Posted By resistor Mar 10, 2022 03:53:00 AM
Found In Egroup: Networks
\ view thread
capture of Code 16#FD02 may be deceiving . Since when power is cycled, Adapter takes time to establish connection with PLC .I believe PLC captures that code during this initiation . Chassis is up now for more than 24Hrs, knock on the wood. Contacted AB support as well and they pointed out that local ...
Posted By resistor Mar 08, 2022 09:02:00 PM
Found In Egroup: Networks
\ view thread
I do not have another AENTR under IO configuration though I have another controller under IO for peer to peer communication. That controller has it's own AENTR but do not have connection issue with its controller. Yes, AENTR IP is static. Loss of connection is random. Today it ran error free for 12 hours ...
Posted By resistor Mar 07, 2022 07:48:00 PM
Found In Egroup: Networks
\ view thread
One more info would like to add. Initially adapter connection "Major fault on controller if connection fails while in run mode " was checked and processor was halting. Now when it is unchecked when connection is dropped connection tab shows waiting with error code #0204 . No red light on Adapter. can ...
Posted By resistor Mar 07, 2022 07:33:00 PM
Found In Egroup: Networks
\ view thread
Thanks Ryan taking time to answer. Here's the screen shot of IO tree total six ethernet devices. On remote chassis I have four DC I/O configured with 20ms RPI. though there is a stratix 5400 switch, Remote adapter is connected directly to Controller Ethernet port. When communication to adapter is dropped ...
Posted By resistor Mar 06, 2022 08:32:00 PM
Found In Egroup: Networks
\ view thread
I have 1769-L33ER processor connected to remote rack with 1769-AENTR. Adapter is configured for full duplex auto negotiation. Controller is losing connection with Adapter intermittently with code 16#204 waiting on connection. Only can reestablish communication after recycling the power to adapter. ...