List of Contributions

Zinhar

Contact Details

Zinhar


My Content

1 to 14 of 14 total
Posted By Zinhar Jun 10, 2026 09:10:14 AM
Found In Egroup: Automation Control
\ view thread
Hello Marcel, The issue has now been resolved. I will be granted access to Technot shortly. I am using Windows 10 Pro OS, with FactoryTalk View Studio v16 installed, and I had installed the May 2026 Patch Rollup. Previously, even after disabling HTTPS, the DataLogPro page was still not opening. I ...
Posted By Zinhar Jun 10, 2026 08:56:14 AM
Found In Library: Automation Control
Posted By Zinhar Jun 10, 2026 08:56:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Ajay, Thank you for your support. Unfortunately, I do not have access to Rockwell Knowledgebase, so I was unable to open the referenced TechNotes. However, I have now resolved the issue. The root cause was related to HTTPS configuration. I reviewed all FactoryTalk View SE projects in FactoryTalk ...
Posted By Zinhar Jun 09, 2026 07:24:03 AM
Found In Library: Automation Control
Posted By Zinhar Jun 09, 2026 07:24:00 AM
Found In Egroup: Automation Control
\ view thread
Hi all, I am using FactoryTalk View SE v16 and I am facing an issue where DataLogPro does not open in FactoryTalk View Studio. I already tried disabling firewall and HTTPS but it didn't help. I found TechNote BF30550, but the link is not available. I would be grateful for any advice. ------- ...
Posted By Zinhar Mar 18, 2026 05:02:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello @Suryawanshi, thank you very much. Yes, you may also invite Philip Hamilton. This matter is very important to me. ------------------------------ [Zinhar] [Osmanlı] ------------------------------
Posted By Zinhar Mar 17, 2026 06:31:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, In Studio 5000, I have developed a model using the PlantPAx tasking model. I am using various instructions such as PAI, PAO, PDI, PDO, PMTR, PPID, PVLV, etc. All of these blocks have Limit_Status outputs. For example, the Analog Input (PAI) instruction includes status bits such as Sts_Lo, Sts_LoLo, ...
Posted By Zinhar Jan 28, 2026 07:02:00 AM
Found In Egroup: Automation Control
\ view thread
We would like to ask for your recommendation regarding an Allen-Bradley graphic terminal that can be integrated into a Honeywell EtherNet/IP DLR network. Currently, the existing network consists of Honeywell HC900 redundant controllers with EtherNet/IP Remote I/O modules, operating in a DLR (Device ...
Posted By Zinhar Jan 05, 2026 05:15:28 AM
Found In Egroup: Automation Control
\ view thread
Hi, Based on the technical specifications, it is understood that ACM automatically removes slots above 10 because the ControlLogix 5590 Process Controllers are XT-rated, and previous generations of XT controllers supported only 10-slot chassis configurations. However, we would like to receive an explicit ...
Posted By Zinhar Dec 25, 2025 12:08:00 PM
Found In Egroup: Automation Control
\ view thread
Hello everyone, I am facing an issue related to Studio 5000 Application Code Manager (ACM). When I place ControlLogix 5590 controllers into 13-slot or 17-slot chassis and generate the controller using ACM, the generated ACD file only keeps the first 10 slots. The remaining 3 or 7 modules (slots above ...
Posted By Zinhar Nov 18, 2025 06:53:00 AM
Found In Egroup: Installation & Activation
\ view thread
When installing Application Code Manager V4 or V5, an error occurs when the SQL installation is completed and the Installation fail message appears. Operating System Windows 11 Pro 23H2. How can I fix this? EDIT: moved to Installation & Activation community -FL ----------------------------------- ...
Posted By Zinhar Nov 18, 2025 06:52:55 AM
Found In Library: Installation & Activation