List of Contributions

sahabat inti

Contact Details

sahabat inti


My Content

1 to 20 of 50+ total
Posted By sahabat inti Jul 21, 2026 06:02:21 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Luca, I'm trying to make a SCADA table that will be accessed in eChart, so the query will be easier to manage but if there's no other way then I will do it with different table for each meter then thank you, Brian
Posted By sahabat inti Jul 20, 2026 11:18:24 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Shilok, I think it would be better if you use scale layout to do this, just change the Font Scaling to true It will change the font when you change the width and length of the window Regards, Brian
Posted By sahabat inti Jul 20, 2026 09:05:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, All I'm having errors writing multiple loggers to a single table I'm trying to log around 100 power meters, the table design : Timestamp, LocalTimestamp, Id, Meter_Id, kWh, kW, V1, V2, V3 so I created 100 loggers for each meter, I only activated around 22 loggers for now, and it said 2 loggers ...
Posted By sahabat inti Jul 14, 2026 08:55:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, Sorry for late reply I've been quite busy lately Here's a google drive link for the project You can change the color of the bar in the js files or you can do it using c# in Optix https://drive.google.com/file/d/1Ds8KU7KmKCCOyubgC3_skgjONVkAev2y/view?usp=sharing regards, Brian
Posted By sahabat inti Jul 12, 2026 08:35:44 PM
Found In Egroup: FactoryTalk Optix
\ view thread
no problem man let me know if you need an example for the eChart
Posted By sahabat inti Jul 09, 2026 10:39:12 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I ended up using Apache EChart to tackle this issue Do you need an example of it?
Posted By sahabat inti Jul 02, 2026 02:07:24 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I also made a mistake of updating the VS the workaround is to File -> Open -> Project/Solution and open the sln file of your project
Posted By sahabat inti Jun 16, 2026 08:53:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Jacek, Do you mean the pipes you have now are a bit disarray? could you send the project files instead?
Posted By sahabat inti Jun 11, 2026 10:05:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
The component you're looking for is Scale Layout By putting all your other components into a Scale Layout it will automatically shrink or enlarge the scaling of each item Make sure you change Font Scaling to true so text also gets scaled Change the Fill Mode to either Fit or Stretch, Stretch ...
Posted By sahabat inti Jun 11, 2026 10:04:51 PM
Found In Library: FactoryTalk Optix
Posted By sahabat inti May 20, 2026 05:56:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I want one... but not in US, now I'm sad -------------------------------------------
Posted By sahabat inti May 17, 2026 08:29:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I take the FT Optix Community Creed! -------------------------------------------
Posted By sahabat inti May 12, 2026 08:29:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Ash, thank you for the suggestion, I will look into it but I'm gonna need to take a picture from the clients tablet and upload it to the server what I need is to insert meters value such as flowmeter and log it into the database and then take a picture as a proof of the reading I guess I would ...
Posted By sahabat inti May 06, 2026 08:38:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
thanks, will be waiting for that feature then -------------------------------------------
Posted By sahabat inti May 06, 2026 04:52:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi all, I am trying to make a project where I could upload images from the client PC/Tablet to the server Project Folder has anyone ever tried doing this? Regards, Brian -------------------------------------------
Posted By sahabat inti May 05, 2026 02:56:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
sweet, great you got it regards Brian -------------------------------------------
Posted By sahabat inti May 03, 2026 09:08:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, Delgado I think you can just make the Visible property to true or false to show or hide the image instead of changing the opacity Regards, Brian -------------------------------------------
Posted By sahabat inti Apr 10, 2026 05:39:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Dex, Everything is working awesome thank you again for your help I really appreciate it! Regards, Brian -------------------------------------------
Posted By sahabat inti Apr 08, 2026 06:36:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Dex, Thanks for your reply could you pass me the pdf? I tried changing the parameters and it works I used output frequency to all DL To Net parameters and PF755_I change to it Thank you, Brian -------------------------------------------
Posted By sahabat inti Apr 08, 2026 04:04:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Dex, I finally change the PLC to 20LE-QWB I can use the Class1 with Dlinks could you teach me on how to change/assign the Datalinks parameters? is Parameter 0,1,2 already fixed? from what I know by reading the program, parameter 2 is the speed feedback So, I need to change the 16 other parameters ...