List of Contributions

Lgcelx

Contact Details

Lgcelx


My Content

1 to 4 of 4 total
Posted By Lgcelx Sep 16, 2025 04:21:00 AM
Found In Egroup: Automation Control
\ view thread
Hi to all, i would like to make cross reference of a variable like L1_gen.linea.stz[1].ds[2].val but it doesn't work. I have seen that it is possible to use the search command but it is too slow. Is there some options for to solve this? -------------------------------------------
Posted By Lgcelx May 08, 2024 09:43:00 AM
Found In Egroup: Automation Control
\ view thread
Hi to all, i have a mobile view panel. I need to open a page with the same button but the number of page change e depend from a tag. How i can implement this functions? Many thanks to all.
Posted By Lgcelx Mar 28, 2024 10:54:00 AM
Found In Egroup: Automation Control
\ view thread
Hi to all, i have a project made two years ago with studio 5000 V33.00. Now i have to open this project and made a new project with studio V36.01. When i open the old projet, some ADDON are converted because some plc instruction with the version V36.01 are changed (see the picture). ...