List of Contributions

David King

Contact Details

David King


My Content

1 to 11 of 11 total
Posted By David King Jun 12, 2024 11:51:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you Glados! ------------------------------ King ------------------------------
Posted By David King Jan 26, 2024 05:01:00 AM
Found In Egroup: Automation Control
\ view thread
They're just not willing to concede the point: Hopefully somebody here has more pull with Rockwell because this is highly irritating, especially considering what we pay for their software and processors. @Philip Hamilton do you have any insight on this?
Posted By David King Jan 25, 2024 11:36:00 AM
Found In Egroup: Automation Control
\ view thread
I'm with ABUser54321, It only affects the 5380 processors, I doubt that's by design.
Posted By David King Jan 25, 2024 09:53:00 AM
Found In Egroup: Automation Control
\ view thread
Well, here's Rockwell's response:
Posted By David King Jan 05, 2024 01:04:00 PM
Found In Egroup: Automation Control
\ view thread
Here's the Keyence IV3 EDS. The IOLink masters that were mentioned were also directly downloaded from IFM and Keyence's websites. ------------------------------ David King ------------------------------
Posted By David King Jan 05, 2024 01:03:33 PM
Found In Library: Automation Control
Posted By David King Jan 04, 2024 12:20:00 PM
Found In Egroup: Automation Control
\ view thread
I opened the EDS with EZ-EDS and the maximum value for both the input and output UINTs is 65535, I changed the max to 32767 (the max for a signed), reinstalled the EDS, still no luck. Hopefully we can get some direction from Rockwell. ------------------------------ David King ---------------- ...
Posted By David King Jan 04, 2024 07:55:00 AM
Found In Egroup: Automation Control
\ view thread
One thing I've noticed once you have V36 installed, with a 5069 controller, even in V35, when you create an ethernet module the I/O data is no longer in an array. If you import an ethernet module the tags are imported in an array format. This new format causes existing AOIs to not function. I'm ...
Posted By David King Dec 27, 2023 03:24:00 AM
Found In Egroup: Automation Control
\ view thread
The Ethernet modules will not connect (yellow triangle in the controller tree). But I can see the devices in linx and ping them. ------------------------------ David King ------------------------------
Posted By David King Dec 26, 2023 04:40:00 PM
Found In Egroup: Automation Control
\ view thread
I'm curious if anyone else is having problems with ethernet modules in V. 36? We just upgraded a work cell from a guard logix L43S to 5069-L340ERS2. I'm having trouble with 1 of the 3 ABB robot generic ethernet module and a keyence NQ-EP4L IOLink master via EDS. We have these deployed all over our plant ...
Posted By David King Nov 09, 2021 10:39:00 AM
Found In Egroup: Automation Control
\ view thread
I'm trying to set up a USB badge reader to have operators log in. I'm struggling to find the value entry method for text input that the help file says I can change to "inline" so it will accept a USB keyboard input instead of the virtual keyboard. Has anyone successfully integrated a USB keyboard or ...