List of Contributions

Reino

Contact Details

Reino


My Content

1 to 20 of 50+ total
Posted By Reino Jan 07, 2026 01:05:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Ramakrishnan, If you call tech support they should be able to help you with some scripts. Thanks, Dan ------------------------------ D Reinarts ------------------------------
Posted By Reino Nov 12, 2025 06:21:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Ramakrishnan, The selection of filters you have is likely appropriate for your application. It is feasible to have that much data in a complex application with a lot of report parameters. I would evaluate what information you are collecting by going through a journal file. There are database tools ...
Posted By Reino Nov 11, 2025 01:11:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Ramakrishnan, I would not send a journal file on an open platform. I suspect the batch system is collecting the information correctly. There are tools to manage the database, look in the following folder C:\Program Files (x86)\Rockwell Software\Batch Database Utility\Batch Database Manager. ...
Posted By Reino Nov 11, 2025 08:05:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Ramakrishnan, It would be good to know what is being logged as 300,000 records does seem high for a batch. I would start by trying to determine if it is the batch system or the archiver that is causing excessive records. Is the batch system setup for "End of Batch" or "Incremental"? this can ...
Posted By Reino Sep 29, 2025 04:14:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Dennis, Dennis, On Server 2022 the security it tighter around the folder structure. Because you could copy 1 schema file your user must have rights to place a file in that folder. I'm not sure why the files are not showing up during the install or the copy(from your video), I would right click ...
Posted By Reino Sep 27, 2025 09:01:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Dennis, Just checking to see that your installation is ok. Normally if there is a problem with the material server installation the log file will indicate that it cannot communicate to the Material server. The error you are getting indicates that you are not pointing to a valid area model or the ...
Posted By Reino Sep 26, 2025 07:03:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
For the Code Meter issue look at technote BF25378. For the batch issue can you set the area model back to the ice cream demo? Below is a snapshot of what it should look like in server options, If you have Material Manager installed you will need SampleDemo2. FTBatch15 should be your computer na ...
Posted By Reino Sep 25, 2025 02:51:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Paul, I checked on version 17 and the MasterRecipe.XSD file does not exist. You may be able to call technical support to see if they have one. I have seen a shift from attempting to create master recipes from general recipes via XML to creating formulations in MS SQL Server. I realize this ...
Posted By Reino Sep 25, 2025 01:42:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
PickleMan, For the activation it is indicating with the red explanation point that it is not happy. I would hold the mouse over the red ! to see what it says. I might try putting the IP address just to see if it behaves different. For the batch issue I would look at the Batch server logs (BATCHSVR.LOG). ...
Posted By Reino Sep 25, 2025 01:20:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Alex, There are a few different methods for collecting exception events and I am only looking at this from a reporting perspective (no signatures, corrective action, etc.) RA provides an exception reporting page in the enhanced batch reporting which I believe goes back to version 12 with the 090-Batch ...
Posted By Reino Sep 09, 2025 06:52:00 AM
Found In Egroup: Installation & Activation
\ view thread
What you are seeing is normal. The Feature Version should not make a difference in the RSLinx Gateway product. ------------------------------ D Reinarts ------------------------------
Posted By Reino Aug 28, 2025 10:34:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Dunwoody, I have found the following potential issues. HTTPMethodsPOST_Resouce: could be case sensitive '/api/v1/jobs' I expect this to be ok. raC_LD_HTTP_Client_UserAgent: cannot contain a null character $00 A port could be eaten by another application. If you are running the rest ...
Posted By Reino Aug 26, 2025 10:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Dunwoody, I did take a look to see why the port number would have been removed but didn't find anything yet. I do have a couple of additional questions: Which controller are you using? Did you create your app manually or did you use Application Code Manager? ------------------------------ ...
Posted By Reino Aug 25, 2025 09:18:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I believe you have an extra comma at the end of your payload after the "BestBeforeDays":"8" The rest API server may be able to handle this but I'm not sure the controller can so please try again after removing the comma. ------------------------------ D Reinarts ------------------------- ...
Posted By Reino Aug 22, 2025 09:41:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Dunwoody, In my application I had the port number in the URL. IE: 'http://192.168.1.10:5003' I did struggle initially getting the settings to match what my client needed so there is some trial and error but once it was working for me I had no issues. For the Client_UserAgent I have added ...
Posted By Reino Aug 21, 2025 10:42:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Dunwoody, The group would need a little more information to know if they would want to tackle this question. Are you trying to use an API Key or HTTPS with a certificate? I recommend avoiding encryption and having the printer and controller front port connected directly to the printer as your security. ...
Posted By Reino Aug 07, 2025 04:11:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Yes, there are a couple of ways that I can think of to do this. It is always possible to write a script to query the database and put it into a model tag. If you don't want to write code you can use a data control (A list box is a good choice but can work with others just note it will be on ...
Posted By Reino Jul 22, 2025 09:01:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Not sure how to display the array index in the data grid. I have attached some sample code that loops through an array tag, it is only for single dimensional arrays. aNodeID is a variable added to the script in Optix and is the node ID of the array tag. You will need to add using system.collections to ...
Posted By Reino Jul 17, 2025 10:52:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
DeBruler, Try changing the data type of the variable to BaseDataType. Then the data type should not matter. ------------------------------ D Reinarts ------------------------------
Posted By Reino Apr 04, 2025 08:39:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
You just need to install the latest version and open the project and it should upgrade everything. Please note that the old version is not uninstalled, you will have to manually uninstall the old version unless you want to keep it. ------------------------------ D Reinarts ------------------- ...