List of Contributions

evanmars

Contact Details

evanmars


My Content

1 to 6 of 6 total
Posted By evanmars Jan 24, 2025 12:33:00 PM
Found In Egroup: Legacy
\ view thread
If you are also migrating to a CompactLogix, there is no need for a gateway.
Posted By evanmars Jun 13, 2024 07:10:00 AM
Found In Egroup: Legacy
\ view thread
Check out PLX51-DF1-ENI
Posted By evanmars May 17, 2024 09:18:00 AM
Found In Egroup: Legacy
\ view thread
Thanks GLaDOS. Purchased a Prosoft AN-X-AB-DHRIO
Posted By evanmars May 16, 2024 08:17:00 AM
Found In Egroup: Legacy
\ view thread
I currently have a SLC 5/04 communicating through DHRIO to a PanelView 1000e. Would like to upgrade the HMI to a PV+ 7 What would be the best way to do this, if it is even possible?
Posted By evanmars Apr 26, 2023 07:55:00 AM
Found In Egroup: Legacy
\ view thread
Ah, yes. Thanks. It's been so long since I've worked with a SLC (nearly 20 years ago!), I forgot about the direct reference since everything else on this HMI was done with tags. ------------------------------ evanmars ------------------------------
Posted By evanmars Apr 25, 2023 02:04:00 PM
Found In Egroup: Legacy
\ view thread
Is it possible to read a complete I/O module word at once in the PV+ 7, instead of bit by bit. i.e. I want to read I:1.0, I:2.0, etc. Trying to make I/O status screens but I don't want to have to make 448 discrete tags. Would prefer just 28 tags then mask and shift to get the bit I'm looking for. ...