Using a SMC 150-F480N Ser B for starting / stopping a 354Amp chipper motor. using Devicenet for control I am having trouble with SMB stopping. command it to stop using Option Input #1 set high then low. For about a minute the motor is braking fine (display shows stopping) then it sounds as if it is running ...
|