List of Contributions

Ton

Contact Details

Ton


My Content

1 to 20 of 20 total
Posted By Ton Aug 04, 2025 10:50:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
It does not seem like to like the UDT or structure from the PLC. If I create a model with the variables I want to use and convert that to a type. Use that as the alias then it seems to work. I cannot get it work using the type that is coming directly from the PLC. I can not also browse to some of sub ...
Posted By Ton Aug 04, 2025 09:15:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I removed the variable on the base object and added an Alias of kind equal to the PLC udt. Then referenced the alias in all the objects inside. I then added to the screen and pointed alias to the PLC tag. It still does not work. -------------------------------------------
Posted By Ton Aug 04, 2025 08:11:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I am creating a base object for interface to a device that we can use over and over again. I created a panel with a variable that is a structure of type from the PLC that has all the information we need for this device. Inside the panel I created several push buttons with indicators and text tied to ...
Posted By Ton Jul 16, 2025 07:57:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Does this only work on the actual hardware. I tried running it with echo and emulator and it says it cannot run the modules.
Posted By Ton Apr 04, 2025 09:45:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I compared a project that does not give this error with the one that is in notepad and do not really see why this one is having this issue. Is there somewhere where you could tie a dynamic link to version? I cannot find it
Posted By Ton Apr 04, 2025 09:35:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Project: Name: EdgewaterTemplate GUID: 0e86c09fb5e87ff79edd6eeef1c993ba ProjectNamespaceIndex: 18 Description: '' Company: '' Copyright: '' FormatVersion: 1 ProductVersion: 1.5 CoreVersion: 4.0 Dependencies: 2: Uri: 'urn:FTOptix:Core:Net' Module: FTOptix.Core.Net Version: ...
Posted By Ton Apr 04, 2025 09:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I am uninstalling the older versions. I am not using them.
Posted By Ton Apr 04, 2025 09:27:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have 3 versions installed but using 1.5.6.0 and version text file says 1.5.6.0-Stable
Posted By Ton Apr 04, 2025 09:18:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
it also seems like it will not allow me to change the IP address of the commdriver I change it and when I open it back up it goes back to the old address.
Posted By Ton Apr 04, 2025 09:14:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have attached the log file. When I hit save file I get this message. I am also getting these errors. I am using echo to test and I am able to go online with it ok in studio and it browses tags ok. The IP address in the driver is set correctly at 172.16.182.131 but it is still showing old ...
Posted By Ton Apr 04, 2025 09:13:53 AM
Found In Library: FactoryTalk Optix
Posted By Ton Apr 04, 2025 08:28:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I keep getting this error message. What does this mean? How do you correct this? EDIT: modified title to include product name -FL
Posted By Ton Feb 26, 2025 01:44:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I must be since I see the alarm tags import ok and if I do a default alarm in optix triggered off a bit it works ok. I just do not get the factory talk alarms to show up.
Posted By Ton Feb 26, 2025 12:43:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
No they are alarm based tags inside studio 5000. The same type you would use for a 5500 display in the past. I trigger them but I do not get a alarm in Optix. I am using emulator with echo but still should work?
Posted By Ton Feb 26, 2025 12:40:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I do not get the option to import alarms.. Is there something else I need to enable to do this?
Posted By Ton Feb 26, 2025 12:10:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I have created several alarm tags in the PLC program, I also added them as tags to optix. What do I do to setup Optix to trigger alarms off of these tags when they go active. I am using Echo and emulator right now as well.
Posted By Ton Jan 29, 2025 07:24:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
How do you tie the fill level of an object such as a tank or box to a tag. So, as the tag increases the object appears to fill up. Would like to create a simple rectangle box that I can fill horizontally as value increases.
Posted By Ton Jan 16, 2025 01:44:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
So each button uses a key convertor for the color of the button. You also have the boolean for each button as the command. Can you create a udt inside optix that contains a tag for the boolean as well as the key convertor reference. Then on the top of the button add a variable of that type. ...
Posted By Ton Jan 16, 2025 12:48:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I am looking to create a library of objects in Optix. One of the items in the library are buttons that had a color key for the background. Is there a way to create a object with alias tags for button push and color key that I can place in a library. Then I can drop them in a project and connect ...
Posted By Ton Jan 16, 2025 07:45:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
How do you change the background color of the data entry? I do not see a property to change this?