List of Contributions

Eric Arsenault

Contact Details

Eric Arsenault


My Content

1 to 17 of 17 total
Posted By Eric Arsenault Apr 11, 2025 11:21:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
So I have always been able to access SNMP data of the 1756-EN2T for monitoring networks, but now with FW 12.001 I am unable to access any SNMP data. (See images attached) Has anyone had similar issues? So far Tech Support has not provided any more information, only that nothing has changed with SNMP ...
Posted By Eric Arsenault Aug 30, 2024 11:49:00 AM
Found In Egroup: Automation Control
\ view thread
I too have had this, but have discovered the path was being set in other versions of the software. I cannot remember what version ruled where the file was saved, but I had to modify the path in another version then it took effect in the version I was working with. so if you have multiple ...
Posted By Eric Arsenault Aug 27, 2024 06:06:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I have the following firmware on net network that has had the NET IO TimeOuts / Link Down 1756-ENBT 6.006 755TM Common Bus 12.001 755TM Common Bus 12.001 755TR Regen Bus Supply 12.001 I am not a drive specialist, but in the above configuration, there is a dedicated fiber link between the three ...
Posted By Eric Arsenault Aug 23, 2024 11:22:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
More information The PF755T drives that have had NET I/O timeouts on, are connected through a 1756-ENBT F/W (6.06) The other PF755T drives that we have not had this issue with are connected through 1756-EN2T modules F/W (11.02). Hey, @Splash, Are your drives connected via ENBT or EN2T?
Posted By Eric Arsenault Aug 23, 2024 09:40:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
All Drives are set to 100mS, All Devices are UniCast.
Posted By Eric Arsenault Aug 23, 2024 09:05:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
We have 3, 755T drive that have been installed and in use for about 80, but yesterday all three lost communications at the same exact time (within 2 seconds of each other from our PLC). The managed switch reported link down and up at time of event for approximately 2 seconds. On the same network 7 PF753 ...
Posted By Eric Arsenault May 02, 2024 04:24:00 PM
Found In Egroup: Advanced Software
\ view thread
It does work as chrome published as an rds app. I have gotten a reply from Rockwell tech support that sound does not currently work in a container.
Posted By Eric Arsenault May 01, 2024 08:42:00 AM
Found In Egroup: Advanced Software
\ view thread
Been trying to get sound to work for three days, using a chrome container. I know I can output sound from the unit if using a remote desktop client, but no sound coming from the chrome container. Have tried different hardware clients. (Onlogic and PXE). Awaiting a response from tech support if ...
Posted By Eric Arsenault Mar 22, 2024 06:50:00 AM
Found In Egroup: Advanced Software
\ view thread
I have had similar issues at different sites like you describe. In my experience, I have had to disable POE on the network port and / or force the port speed to fixed at 100M. Typically, just disabling the POE works.
Posted By Eric Arsenault May 23, 2023 07:33:00 AM
Found In Egroup: Advanced Software
\ view thread
As it turned out to be a POE @ 1000M connection that was preventing the TM120 units from booting. Once disabling the POE on the switch these units booted properly. We have also tested with the VersaView 6300T (6300-BBB2DA) units and get very similar results. Disabling the POE allows these units also ...
Posted By Eric Arsenault May 05, 2023 12:07:00 PM
Found In Egroup: Advanced Software
\ view thread
Edited to correct Stratix typo - to aid in search discovery. I have an open ticket with rockwell, but am reaching out the community if anyone else is experiencing similar issiues. At two different facilities (Differnet installs of thinmanager both at v13.1), we are experience problems with OnLogic ...
Posted By Eric Arsenault Jun 07, 2022 03:13:00 PM
Found In Egroup: Automation Control
\ view thread
So did more testing and when changing the IP address of the drive, CCW see this as a parameter change in the Drive and flags for an upload, This puts the asterixis in the program and saves the "new" project path. When NOT changing the IP address, but the path of how the software accesses the drive, it ...
Posted By Eric Arsenault Jun 07, 2022 03:01:00 PM
Found In Egroup: Automation Control
\ view thread
fuzzy logic, I preformed the same test in my lab environment with different results. We use CCW 20.01 and FTLinx 6.30. When clearing the path the * never appears next to the drive. Attempt 1 1a) New Project, Discovered the drive(PF525), added it to the project saved the drive and closed. Drive ...
Posted By Eric Arsenault Jun 06, 2022 06:54:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you Ron, This has addressed my original issue of opening the CCW project and being able to get online for different PC's. I just need to remember to always utilize FTLinx. As a follow up question you mention "First, its generally a good practice to force a save of a path with a project once ...
Posted By Eric Arsenault May 31, 2022 12:36:00 PM
Found In Egroup: Automation Control
\ view thread
Ethernet to VFD. From PC over Ethernet. I can discover using either RSLinx or FTLinx. When reconnecting to the drive from a saved project, it can be hit or miss, most of the time it will not reconnect. It will never reconnect if opening the saved project on a different PC. Even ...
Posted By Eric Arsenault May 16, 2022 02:23:00 PM
Found In Egroup: Automation Control
\ view thread
In the newer versions of CCW when connecting to a Drive from a different computers, we always have to clear communications path and re-browse to establish communications to the drive. Even when the Path is technically the same. I believe in older versions it would prompt the user that the path was incorrect ...
Posted By Eric Arsenault May 10, 2022 03:19:00 PM
Found In Egroup: Automation Control
\ view thread
So did Rockwell really go from version 13 to version 20 ?