List of Contributions

Ceelen

Contact Details

Ceelen


My Content

1 to 5 of 5 total
Posted By Ceelen Jun 25, 2024 04:05:00 PM
Found In Egroup: Legacy
\ view thread
The HMI only sets the bit, the PLC resets it. The remote bit does stay in longer than the local, I'm thinking because the two are connected via ethernet switch and ETAP's. No undesirable consequences for the logic however.
Posted By Ceelen Jun 25, 2024 03:58:00 PM
Found In Egroup: Legacy
\ view thread
I wanted to reply and thank both of you for the help. I had to make the edit suggested here, and I completed the other edits for start/stop/purge as well. Everything tested and in service. Great community!
Posted By Ceelen Feb 20, 2024 03:59:00 PM
Found In Egroup: Legacy
\ view thread
Apologies, I thought it would be better to see the file clean without my edits. I did in fact use B54:0/4 in rung 27 in parallel as an XIO. Your suggestion to instead put it in series will probably solve my issue. I will follow your advice and update this post.
Posted By Ceelen Feb 20, 2024 11:03:00 AM
Found In Egroup: Legacy
\ view thread
Hello All If I should be posting to a different community, let me know. I am looking for a little help adding some remote functionality to a already existing compressor panel program. Runs on RSlogix 500. Basically, allows for our operations group to Start/stop and reset alarms and S/D's without ...
Posted By Ceelen Feb 20, 2024 11:02:40 AM
Found In Library: Legacy