List of Contributions

efla_dadi

Contact Details

efla_dadi


My Content

1 to 16 of 16 total
Posted By efla_dadi Sep 10, 2024 01:46:00 PM
Found In Egroup: Networks
\ view thread
Hello I am using Control Logix controller 1756-L82ES with network card 1756-EN2TR for my IO network that consists of several 1734-AENTR modules connected in DLR. The question is, Can a switch that supports HSR protocol (but not DLR) be added to the DLR ring? These two protocols seems to ...
Posted By efla_dadi May 03, 2011 05:38:00 AM
Found In Egroup: Advanced Software
\ view thread
Gentlemen I am migrating a project from RSView 4.0 to FTView SE 6.0 and I have this error when creating the redundancy of the hmi server: failed to retrive the version of the hmi server I have chcked the isapi dll files in the project of both pri and sec machine folder and they have the same version. ...
Posted By efla_dadi Apr 07, 2011 10:18:00 AM
Found In Egroup: Automation Control
\ view thread
It is solved.......I uninstall studio and installed it again and everything works fine. Thanky you for your postings ##HL40
Posted By efla_dadi Apr 07, 2011 05:08:00 AM
Found In Egroup: Automation Control
\ view thread
Like I told in my posting " I have checket the permissions to the folders that are used." So this technote I have allready checked. Can it be of wrong setup of IIS? ##HL40
Posted By efla_dadi Apr 06, 2011 09:23:00 AM
Found In Egroup: Automation Control
\ view thread
I forgot to mencion that the new system with FTView 6.0 is a windows server 2008 system. ##HL40
Posted By efla_dadi Apr 06, 2011 09:09:00 AM
Found In Egroup: Automation Control
\ view thread
Summary: Problem creating HMI server from RSView 4.0 application to FTView 6.0 application I am upgrading scada system from RSView SE 4.00 (CPR7), running on WindowsServer 2003 to FTView 6.00 (CPR9 SR3). I am having problems with the *.gfx files. When creating the HMI server and importing the hmi ...
Posted By efla_dadi Mar 02, 2010 04:34:00 AM
Found In Egroup: Automation Control
\ view thread
I have one rack with ethernet FLEX IO 1794 - AENT/A (Chassis Size 8 Rev. 2.1) connected to 1756-L63 (Rev. 15.4) Processor through eth 1756-ENBT/A (Rev. 3.9). In this rack I have 8 modules, 6 pcs. 1794-IB16/A modules and 2 pcs. 1794-IRT8 modules. The terminal base that are used for the 1794-IB16/A modules ...
Posted By efla_dadi Aug 31, 2009 04:05:00 AM
Found In Egroup: Automation Control
\ view thread
Hi. Do you know of any tool or way to convert RSView datalog file from to a excel file? I want to read the tagname and its value in excel over a time period. Would be great if you know if this is possible. ##HL40
Posted By efla_dadi May 14, 2009 06:22:00 AM
Found In Egroup: Automation Control
\ view thread
Well gyus, problem solved. After checking and tested all the sockets, we take a look at the IO modules. In this rack I have 6 pcs. 1794-IB16 and 2 pcs. 1794-IRT8. All the modules in this rack was faulted. And the strange thing is that all the lights on the modules was working fine, both the IB16 and ...
Posted By efla_dadi May 13, 2009 03:03:00 AM
Found In Egroup: Automation Control
\ view thread
Thanks guys. I will shoot for the bended pins in the sockets. I will get a magnifier and a flashlight to envestigate. I will write the soulution if it will be a success. Regards Dadi. ##HL38
Posted By efla_dadi May 12, 2009 06:37:00 AM
Found In Egroup: Automation Control
\ view thread
I have a problem on my ethernet flex IO. I have ethernet flex IO 1794-AENT module. I replaced a a module that was faulting, the new module has the same revisions (SER A, F/W REV 2.12) except for that the old module has the REV A01 but the new one have the REV A02. All my IO modules have the error ...
Posted By efla_dadi May 06, 2009 09:58:00 AM
Found In Egroup: Advanced Software
\ view thread
I am using RSView SE, Version 4 CPR7. Is it possible to use two or more AREAS, in one application in a redundant system? Under each area I am planning to have one hmi server and one data server. Application Area_1 HMI_server_1 Data_server_1 Area_2 HMI_server_2 Data_server_2 ...
Posted By efla_dadi Apr 14, 2009 09:19:00 AM
Found In Egroup: Automation Control
\ view thread
Ok, thanks. I have a plan to test this setup. I will keep this open, if anyone have tested this setup. I will reply the result if it was a nuclear meltdown or a success:smileyvery-happy: ##HL40
Posted By efla_dadi Apr 14, 2009 09:00:00 AM
Found In Egroup: Automation Control
\ view thread
Is RSView Studio 4, CPR7 supported with Microsoft operating system Windows Server 2008? ##HL40
Posted By efla_dadi Apr 03, 2009 08:08:00 AM
Found In Egroup: Advanced Software
\ view thread
In a redundant system I have active and standby macros to control which server is in charge. Shall the AlarmOn command be in both the active and the standby macro? Shall the alarm be on on both the primary and the secondary server? ##HL40
Posted By efla_dadi Mar 03, 2009 09:17:00 AM
Found In Egroup: Automation Control
\ view thread
Hi all. I needed to format my drive on my VersaView 1500P display and now I need the drivers for the display. Can anyone point to a location where I can get those drivers. Thanks. ##HL41