List of Contributions

Nava

Contact Details

Nava


My Content

1 to 20 of 36 total
Posted By Nava Nov 13, 2025 05:04:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi. I did a little HMI project with trends and alarms broswer. Since these two last features are done with scripts, I m not able to see where time is kept from. I would like to add a label with the day and time in it. Where should such label be linked to ? Thanks and Regards. ------------- ...
Posted By Nava Nov 07, 2025 09:13:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
now is working, but I had to set simply to "toggle" and not on "toggle bit" same issue for "set bit value " and "set variable value". Don t know why... Thanks -------------------------------------------
Posted By Nava Nov 07, 2025 07:33:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi. I' m trying to toggle a bit of a modbus coil with a button . I m able to do so with a label (putting in it 1 or 0) linked to the modbus address of the coil Button is set as follow: events -> method -> commands-> variable commands ->toggle bit input argoment - > variable to modify ...
Posted By Nava Nov 05, 2025 06:48:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I found the way: use a circle with conditional converter -------------------------------------------
Posted By Nava Nov 05, 2025 05:02:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello. When I use a LED, the background is always white (OFF case). Is it possible to change ? thanks -------------------------------------------
Posted By Nava Nov 05, 2025 03:01:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi. I have a label in which is linked a Modbus address. Is it possible to assign or format such label, in the way that beside the numerical value, there is the enigineering units (Kg,s, °C) ecc. ? This is to avoid the tedious process to create another label beside. Thanks ------------------ ...
Posted By Nava Nov 04, 2025 03:40:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
second picture -------------------------------------------
Posted By Nava Nov 04, 2025 03:39:37 AM
Found In Library: FactoryTalk Optix
Posted By Nava Nov 04, 2025 03:36:22 AM
Found In Library: FactoryTalk Optix
Posted By Nava Nov 04, 2025 03:36:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi. I created a trend using the variables stored in a data logger. So is a kind of "history trend". I don't know what variables are going to do in the trend itself: "polling time" & "sampling period" in Data Logger "refresh time" in Trend: changing it I don-t recognize any significant ...
Posted By Nava Nov 02, 2025 04:57:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Dear Asemlucben, thanks for the answer. Anyway I found the reason, that is slightly different this time compared to the one I was explaining in the premises. (may be is already explained in your last answer, but Im quite illiterate about modbus). If I correctly understood, every modbus station has ...
Posted By Nava Oct 20, 2025 11:19:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi. I'm preparing a project with modbus station that contains holding registers and coils. At beggining I had only holding registers and I was not able to read values (of some of them) when I was changing them on the slave. changing them from master (HMI) was detected by slave. I solved this issue ...
Posted By Nava Oct 17, 2025 01:40:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Unfortunately none of your methods has worked. Thanks anyway for your help. -------------------------------------------
Posted By Nava Oct 17, 2025 11:54:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi. Is it possible to have the text of a label with some letter in superscript or others in subscript (I need for engineering units but also for other purposes). Edit: please correct my title of the 3d because I was wrong to make the translation to english. Thanks and Regards. EDIT: corrected ...
Posted By Nava Oct 16, 2025 08:42:16 AM
Found In Library: FactoryTalk Optix
Posted By Nava Oct 16, 2025 08:42:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Dear asemlucben thanks. I subscribed to github, but after inserting the link I got this message " The system has encountered a problem, we are working on it. Please check back later." Can you briefly explain me how to point the trend to the data logger ? I did it but it s not working. Thanks again and ...
Posted By Nava Oct 16, 2025 07:51:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi. I want to create a trend chart, length 1 minute. I would like that every time I refresh the page, this will not go to restart from the moment I recall, but it memorizes with continuity the trend in the last 1 minute. I tried to create a "Data Logger" with the variables of the trend and ...
Posted By Nava Oct 13, 2025 03:36:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Good morning. is it possible to draw the polylines dotted instead of continuous and to put markers (circle or points) at begin and end of each polyline ? Thanks and Regards -------------------------------------------
Posted By Nava Oct 01, 2025 06:36:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello everybody. I seem to have solved the issue by increasing the value "max gap in bytes" (see image in my previous post) but I don-t know what is the meaning (in my case original was 4 ) . i will study over it... Regards -------------------------------------------