Hello Johnson, When you are saying move it means you are using the MAM instruction. You can monitor the .PC bit of the MAM instruction. This bit becomes high when the axis is at the end Position of the move. The PC bit stays set until the rung makes a false-to-true transition. The PC bit stays cleared ...
|