List of Contributions

Johann Kotze

Contact Details

Johann Kotze


My Content

1 to 20 of 50+ total
Posted By Johann Kotze Jul 01, 2026 11:28:00 AM
Found In Egroup: Advanced Software
\ view thread
@Explorer1, Based on the information provided, I recommend starting with the fundamentals and isolating whether this is a tag-resolution issue or a parameter-substitution issue. First, configure the button using the fully resolved tag path rather than parameters: /Area_Data::[PLC002]Test_Sched.OCmd_ECRst[5] ...
Posted By Johann Kotze Jun 25, 2026 02:13:00 PM
Found In Egroup: Advanced Software
\ view thread
To display an image in an ActiveX control from a button click in FactoryTalk View SE, you would typically use VBA tied to the button event. For example, in the button's click event: Private Sub CommandButton1_Click() Me.ImageControl1.Picture = LoadPicture("C:\Images\image.jpg") End Sub Or, if using ...
Posted By Johann Kotze Apr 29, 2026 09:13:00 AM
Found In Egroup: Advanced Software
\ view thread
Ramakrishnan, This behavior is expected. PlantPAx implements its own area‑based security model, which is enforced at the library level. The Alarm & Event (A&E) system does not understand or enforce this PlantPAx‑specific security, so acknowledgements from the Alarm Summary are evaluated only against ...
Posted By Johann Kotze Apr 29, 2026 08:42:00 AM
Found In Egroup: Advanced Software
\ view thread
Mertens, PlantPAx Display and Library Guidelines PlantPAx - Library of Process Objects – Organisation, Ownership and Arbitration PlantPAx – Library of Process Objects – Equipment Phases PlantPAx – Library of Process Objects – Equipment Modules In current PlantPAx Process Object libraries, this ...
Posted By Johann Kotze Apr 28, 2026 11:04:00 AM
Found In Egroup: Advanced Software
\ view thread
Dowling, When I was reading through your description, my thoughts aligned exactly with Marcel’s recommendation to take a look at how the PlantPAx Library of Process Objects handles this use case. Even though you’re using your own object library, PlantPAx serves as a strong reference implementation ...
Posted By Johann Kotze Apr 17, 2026 09:32:00 AM
Found In Egroup: Advanced Software
\ view thread
The number is available on the Rockwell Automation website. Contact Us -------------------------------------------
Posted By Johann Kotze Apr 17, 2026 09:06:00 AM
Found In Egroup: Advanced Software
\ view thread
HAyden, There isn't enough information from the details provided to determine the root cause of the CPU spike on the FTD host. Since the system has been rebooted, the data needed to confirm what drove CPU to 100% may no longer be available. Please contact our Tech Support team so they can ...
Posted By Johann Kotze Apr 15, 2026 11:10:00 PM
Found In Egroup: Advanced Software
\ view thread
FactoryTalk View Alarms and Events Server Settings FactoryTalk Linx Server Settings -------------------------------------------
Posted By Johann Kotze Apr 15, 2026 11:00:00 PM
Found In Egroup: Advanced Software
\ view thread
What you're doing will "mostly work," but it's not a robust or supported way to keep FactoryTalk tag‑based alarms and Logix ALMD/ALMA controller alarms synchronized. In practice, this approach can be difficult to keep fully synchronized because the tag-based alarm engine and the controller-based ALMD ...
Posted By Johann Kotze Apr 14, 2026 08:28:00 AM
Found In Egroup: Advanced Software
\ view thread
Amol, To add to Bruce's solid recommendations. FactoryTalk Linx Error: "The FactoryTalk Directory Server used by the remote computer differs from the FactoryTalk Directory Server used by the local computer" This error indicates that the local computer and the remote system are ...
Posted By Johann Kotze Mar 30, 2026 08:57:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi McEnteggart, To address your direct question first: The ALARM_DIGITAL and ALARM_ANALOG predefined data types cannot be modified. The structure, members, and memory footprint are fixed and part of the controller's built‑in alarming implementation. It's also not possible to create your ...
Posted By Johann Kotze Mar 23, 2026 05:28:00 PM
Found In Egroup: Advanced Software
\ view thread
HogueGregPLC, I'm not sure I'm following your question, so let me clarify how this works conceptually. An event is always triggered by a single input condition, such as a tag value or an alarm condition (for example, trigger0X). Each event definition has exactly one associated message. The extended ...
Posted By Johann Kotze Mar 22, 2026 08:45:00 PM
Found In Egroup: Advanced Software
\ view thread
HogueGregPLC, Yes, the syntax does exist for FactoryTalk View SE in the Event Message Editor. Which version of FactoryTalk View SE are you currently using. This capability was added in FactoryTalk Alarms and Events v6.31. See screenshots below. ---------------------------------- ...
Posted By Johann Kotze Mar 22, 2026 08:31:00 PM
Found In Egroup: Advanced Software
\ view thread
Reference material for Process Boolean Logix Instruction PlantPAx Process Control Instructions PlantPAx Faceplates for Process Controller Instructions PlantPAx Control Strategies -------------------------------------------
Posted By Johann Kotze Mar 17, 2026 01:55:00 PM
Found In Egroup: Advanced Software
\ view thread
John, For this type of issue, I recommend contacting Rockwell Automation Tech Support so they can review the system directly. Based on the description shared so far, there is not enough detail to clearly understand the sequence of actions taken or where the failure occurs. Please consider ...
Posted By Johann Kotze Mar 14, 2026 11:46:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
ID: QA77044 | Access Levels: TechConnect | FactoryTalk View: Changing the Microsoft ODBC driver version for SQL Server used by default ID: QA77047 | Access Levels: TechConnect | FactoryTalk View: Changing the LocalDB version used by default -------------------------------------------
Posted By Johann Kotze Mar 12, 2026 04:50:00 PM
Found In Egroup: Advanced Software
\ view thread
John, If HTTPS is not required in your system, it can be disabled directly using the FactoryTalk View SE Website Setup utility without disabling any FactoryTalk View components or Windows services. From the Website Setup tool, select the FactoryTalk View SE website, click Disable HTTPS, and restart ...
Posted By Johann Kotze Mar 12, 2026 02:10:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi John, I have a few questions to help narrow this down. Have you applied the latest patch roll-up? ID: QA49264 | Patch Roll-up for CPR9 SRx When you installed FactoryTalk View v16, did you select the SSL option? If you selected SSL, did you configure a certificate and bind it to HTTPS? ...
Posted By Johann Kotze Mar 11, 2026 09:43:00 AM
Found In Egroup: Advanced Software
\ view thread
JeremyM, I am not a VBA expert. This topic caught my interest, so I asked an AI tool to explore the question. You may find some of the suggestions below useful. How do I get raw bytes without unexpected preprocessing? Do not use STRING/STR_XX as a binary container for 0–255 byte data when ...
Posted By Johann Kotze Mar 05, 2026 10:19:00 AM
Found In Egroup: Advanced Software
\ view thread
Some information that might also be of value. ID: QA77044 | Access Levels: TechConnect | FactoryTalk View: Changing the Microsoft ODBC driver version for SQL Server used by default ID: QA77047 | Access Levels: TechConnect | FactoryTalk View: Changing the LocalDB version used by default ----- ...