Posted By
Hatem
Aug 28, 2025 02:07:00 AM
Found In
Egroup:
Automation Control
\
view thread
I have an SLC5/05 system connected to a Pro-face HMI. When the controller goes to fault mode (for math overflow for example), certain outputs are still energized. One of these outputs is related to the HMI Tag. When a Tag "B3:9/0" for example in the HMI is "ON" and energizes a certain output in ...
|