List of Contributions

Nilesh Suthar

Contact Details

Nilesh Suthar


My Content

1 to 17 of 17 total
Posted By Nilesh Suthar Feb 09, 2026 09:48:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
We try two different PC, Install and Uninstall. PC#1 upgraded v 1.6 to v1.7 and downgraded back to 1.6 PC#2 installed with v1.6 Project transfer from Both PC yields same outcome. Optix pro entitlement is good and valid. We copied application file (.z) to usb drive, OptixPanel ...
Posted By Nilesh Suthar Feb 09, 2026 08:13:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
we tried Default template (1920x1080) project and OptixPanel template with system widgets - same result. eventually we do want to use process lib 5.20 in production project. can't get pass this basic testing. thanks ------------------------------ Nilesh Suthar ---------- ...
Posted By Nilesh Suthar Feb 07, 2026 09:22:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
we have two identical 21" Std OptixPanel out of the box (mfg. date dec/2025) doing same thing. most frustrating part is RA tech can't figure out what causing "unable to start application" AND OptixPanel does not have well-defined diagnostic logging. ....It's like oh soot I can't start the application ...
Posted By Nilesh Suthar Feb 06, 2026 10:04:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Did not try firmware. did factory reset couple of time. Rockwell tech was remote in today morning, and he didn't bring up anything about firmware. ------------------------------ Nilesh Suthar ------------------------------
Posted By Nilesh Suthar Feb 06, 2026 09:46:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks for the reply. Check box is unchecked. Deleted and re-apply application multiple times. unfortunately, same message pops up. studio log: we even tried using default template instead of OptixPanel template. same outcome. Thanks Nilesh Suthar ...
Posted By Nilesh Suthar Feb 06, 2026 07:29:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Please see result after second factory reset. Unfortunately, not working. Studio Log: Optix Panel info: Please also see latest log file Thanks for the help - Nilesh Suthar ------------------------------ Nilesh Suthar -------------------- ...
Posted By Nilesh Suthar Feb 06, 2026 07:04:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
i will try one more time factory reset and post log here ------------------------------ Nilesh Suthar ------------------------------
Posted By Nilesh Suthar Feb 06, 2026 06:59:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I did factory reset. the log file we are seeing is after the OptixPanel factory reset. ------------------------------ Nilesh Suthar ------------------------------
Posted By Nilesh Suthar Feb 06, 2026 06:43:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Please see attached log file Thanks - Nilesh Suthar ------------------------------ Nilesh Suthar ------------------------------
Posted By Nilesh Suthar Feb 06, 2026 06:11:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, Can someone please help with this issue? Deploying simple single page test application to a brand new out of the box 21" Std OptixPanel from OptixStudio v1.6.4.11 Please see the studio log below. Optix Panel System info: We need to stick to OptixStudio ...
Posted By Nilesh Suthar Sep 26, 2025 05:34:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks AutomateSHANE for the reply. ------------------------------ Nilesh Suthar ------------------------------
Posted By Nilesh Suthar Sep 26, 2025 12:18:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Do we have a "Print" button in FTOptix (release 1.6.2.36) yet...? Idea is to place print button on report/screen/trend/alarms so content can be printed to default printer attached to HMI terminal. suggest any NetLogic workaround would be helpful too. Thanks Nilesh Suthar -- ...
Posted By Nilesh Suthar Dec 18, 2024 10:54:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, Need some help with FTOptix CommDrivers using with Redundant Network card. FTOptix Runtime L (v 1.5.2.13) running on a W11 PC with dual network interface card. NIC-A (for network A) and NIC-B (for network B). Multiple Modbus Station CommDrivers talking to Modbus servers (06). Each ...
Posted By Nilesh Suthar Oct 15, 2024 10:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks for the reply. just quick follow-up question. Is it possible to manipulate Data grid header orientation via C# scripting? ------------------------------ Nilesh Suthar ------------------------------
Posted By Nilesh Suthar Oct 14, 2024 06:21:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Would it be possible to change Data grid header orientation? From horizontal to vertical left, or right? Currently it looks like this, horizontal header at top: Vertical left header may be looks like this: ------------------------------ Nilesh Suthar --------- ...