List of Contributions

Batman

Rockwell Automation

Contact Details

Rockwell Automation

Batman


My Content

1 to 20 of 50+ total
Posted By Batman Jun 11, 2026 08:30:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Did you have a look on this one Kinetix CIP/Integrated Motion Drive's Digital Inputs Used for Generic Inputs (ID: QA53870 | Access Levels: TechConnect)? If it doesn't work for you I can setup a test to verify... ------------------------------ BATMAN 🦇🦇🦇 Please Like the BAT-replies ...
Posted By Batman Jun 05, 2026 07:10:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi JIE, It is really difficult to read the part number. It seems to me something from Eletro Craft. Have a look: https://electrocraft.com/products/gearmotors/ ------------------------------ BATMAN 🦇🦇🦇 Please Like the BAT-replies that you find helpful, and if your query is answered, ...
Posted By Batman Jun 05, 2026 06:48:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Damian, Try using Dual Feedback option, instead of load feedback. Also, please make some trends with ActualPosition, CommandPosition, ActualVelocity and CommandVelocity. Maybe you have disabled position or velocity error on the drive Exceptions? If the drive starts giving current ...
Posted By Batman Jun 05, 2026 06:43:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Patureau. If your intent is to use Registration, you will need to setup the drive input as Registration. Then you will need to use the instructions MAR (Motion Arm Registration), so it makes this input extremely fast (accuracy +/-3 us), and once activated it will log the axis Position and ...
Posted By Batman May 06, 2026 06:45:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Edens, Please try checking the PF527 webpage for warnings. You mentioned the drive is working fine, can you confirm the LED status are RED instead ORANGE? (Green would be the correct color... just checking). ------------------------------ BATMAN 🦇🦇🦇 Please Like the BAT-replies ...
Posted By Batman Apr 29, 2026 02:56:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Volk, As strange as it can seem, a value above 100% on the RSSI is perfectly normal. It is based on a multiplication of factors and can result in a number greater than 100%. You only need to worry if it is consistently below 80%. If you get values bellow 80%, usually means problem with ...
Posted By Batman Apr 29, 2026 02:46:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
My perception is that the .ER and .ERR never go ON because the instruction isn't executed. I am pretty convinced that if you use the .IP on your logic, as suggested previously you will be able to see transitions. When you reach the step 12, make sure you get the .IP to transition to the next ...
Posted By Batman Apr 28, 2026 03:57:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Fritz, that's great news that you can make the system run with the demo script. It means that the Configuration File is valid and works. It means that all motors have correct IP addresses. Can you please have a look at the log files of the HLC (High Level Controller) using the webpage? I would ...
Posted By Batman Apr 24, 2026 07:40:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Fritz, welcome to engage! From the MagneMotion Configurator tool, you can generate the .mmtrk file and open on the NCHost TCP Interface Utility. I did it for you and it looks similar to your layout: Can you ping all motors? Did you program the Masters and the Slaves through the ...
Posted By Batman Apr 20, 2026 04:44:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi HogueGregPLC, This is an important information. When triggered, a MAM will either execute or fault. As a result you'd either see a .PC or .ER. Please try to implement an intermediate step as suggested previously. Trending is a good tool but as it doesn't happen often it may be difficult ...
Posted By Batman Apr 16, 2026 04:54:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I would advise to use the .IP bit to guarantee this instruction have been triggered and move to next step. Another important fact is the the MAM.PC indicates that the Command Position is executed, but your actual position may not be there yet, due to tuning and position error. This is ...
Posted By Batman Apr 14, 2026 11:25:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi HogueGregPLC, Does the axis completes the actual physical movement? Check if the .IP is ON. What do you mean by "shuts down the line"? ------------------------------ BATMAN 🦇🦇🦇 Please Like the BAT-replies that you find helpful, and if your query is answered, please select Reply ...
Posted By Batman Mar 30, 2026 03:02:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Edens, this thread has been solved. Fulk mentioned below: "Issue has been resolved. Problem was mechanical (bad cylinder) causing excessive movement during a certain part of the process. Nothing wrong with servo, cable, motor, connections, grounding, etc." Is there any other point ...
Posted By Batman Mar 20, 2026 03:21:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, I see the Application Set = Torque Prove, but the Application Act = none, showing that the application is set correctly but not active. To become active I would first check the safety, that I see it is in Testing. It is fundamental to fix the safety for the application to become active. Have ...
Posted By Batman Mar 19, 2026 07:40:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thanks. Interesting the bad position count... it is quite high. ------------------------------ BATMAN 🦇🦇🦇 Please Like the BAT-replies that you find helpful, and if your query is answered, please select Reply > Make Best Answer. ------------------------------ ...
Posted By Batman Mar 19, 2026 05:23:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, NET status solit RED indicates network issue (not only duplicated IP). I see from the screenshot you are on 192.168.12.xx. Are the other devices and switches configured correctly to this network, with subnet mask s etc? ------------------------------ BATMAN 🦇🦇🦇 Please Like the ...
Posted By Batman Mar 19, 2026 04:53:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Load observer Bandwidth and Low Pass Filter can certainly help (or worsen) vibration and disturbances. That'd be great to see also the other gains (velocity, position, feed forwards). ------------------------------ BATMAN 🦇🦇🦇 Please Like the BAT-replies that you find helpful, and if ...
Posted By Batman Mar 19, 2026 04:49:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
It is great that you have implemented. You don't need the RUNG 11 on your code, as you only need a MSG tag as per screenshot below: Some parameters are only collected at startup. But please share a screenshot of the result tag, so we can have a look. Thanks ------------------------------ ...
Posted By Batman Mar 19, 2026 04:44:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi diniz, I happen to have an ArmorPowerFlex 35E in the Batcave and have done some other tests: When you unplug the ethernet cable - connection lost - the drive will decel and stop. In this case there won't be LED's on the drive to indicate the fault. On the other hand, if you configure ...
Posted By Batman Mar 18, 2026 09:35:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi diniz, You are right on saying that the connection loss behavior is present only for the 35S. According to the manual Armor PowerFlex 350 AC Drives, the chapter 6 - Safety only applies for the 35S. This chapter specifies the Connection Lost behavior. So you won't have the "Action" tab in Studio ...