List of Contributions

DAF

Contact Details

DAF


My Content

1 to 11 of 11 total
Posted By DAF Jan 13, 2026 10:48:07 AM
Found In Egroup: Advanced Software
\ view thread
Just providing and update for myself and other that may stumble upon this. The roll up did not work either. -------------------------------------------
Posted By DAF Dec 11, 2025 11:25:11 AM
Found In Egroup: Advanced Software
\ view thread
Thank you, I have not installed any roll up so I will give that a try. -------------------------------------------
Posted By DAF Dec 11, 2025 09:00:02 AM
Found In Egroup: Advanced Software
\ view thread
Thank you for the files. I had our instructor test and they said the following: I had been creating new programs because my concern was using an existing program, might have the old profile in it and not doing us any good. I saved the programs you had in the email. Using the test computer I then ...
Posted By DAF Dec 10, 2025 02:45:40 PM
Found In Egroup: Advanced Software
\ view thread
Follow up- we tried installing the latest AOP's and still got the same issue. Studio 5000 36.02.00 installed on top of 36.00.02 and replaced it if that makes a difference. Thank you -------------------------------------------
Posted By DAF Dec 09, 2025 07:22:45 AM
Found In Egroup: Advanced Software
\ view thread
Hi, all of our AOP's are as it was before on 36.00.02 due to the Windows .net framework update that broke this KB5064403 . With the new upgrade from 36.00.02 to 36.02.00, we were hoping the I/O input card getting added would resolve this like mentioned but it is the same issue occurring. Our students ...
Posted By DAF Dec 08, 2025 01:27:54 PM
Found In Egroup: Advanced Software
\ view thread
With still having the issues does this have to do with an outdated AOP after the minor version as it seems rockwell doesnt provide this with minor version anymore? the Which AOP or firmware package should be installed to update I/O module profiles after upgrading to 36.02.00? Will this then fix the issue? ...
Posted By DAF Dec 08, 2025 12:56:03 PM
Found In Egroup: Advanced Software
\ view thread
So we had upgraded to version 36.02.00 and we still have the issue on both Windows 23H2 and 24H2 of Studio 5000 locking up when trying to create/add and I/O card. You stated the release notes fix this but we continue to have the same issue with the different version. How can we resolve this and what ...
Posted By DAF Dec 08, 2025 12:29:17 PM
Found In Egroup: Advanced Software
\ view thread
Thank you for your help and response! -------------------------------------------
Posted By DAF Sep 30, 2025 09:28:00 AM
Found In Egroup: Advanced Software
\ view thread
Thank you so much for your response. So it does look like the KB5064403 is marked as "fully qualified" in the spreadsheet now. I see it does say in one of the columns "Qualified with RA Rollup" September 2025. Does that mean I need to download this "Patch Roll-up CPR9 SRx Sep 2025" on every workstation ...
Posted By DAF Sep 19, 2025 09:17:05 AM
Found In Egroup: Advanced Software
\ view thread
I have a user with this same issue as well. It is interesting as we have about 200 computers able to browser in FTLinx and RSLinx without issue, but this one user cannot browse nodes in FTLinx, yet it is a new image, same OS version. -------------------------------------------
Posted By DAF Sep 19, 2025 09:13:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, I work in IT and wanted to inform users of an issue we found with Studio 5000 v36.00.02 after this months Windows 11 23H2 September Updates in case anyone else is experiencing this. It would be great if Rockwell or windows could release a hotfix for this as right now we had to uninstall the update ...