Posted By
Yang
Jun 25, 2026 07:46:00 PM
Found In
Egroup:
Automation Control
\
view thread
HI . Under the CIP communication protocol, if the communication path only consists of the 1756-EN2T module and the 1756-L7x processor, the Large Forward Open (0x5B) mode with a 4000-byte payload can be adopted for large-capacity data transmission. However, the communication path at the current ...
|