List of Contributions

Lesley

Contact Details

Lesley


My Content

1 to 20 of 48 total
Posted By Lesley Jan 09, 2026 03:34:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Splash, Perhaps the following manual can provide some insights into the capabilities of FactoryTalk Updater. FactoryTalk Updater Getting Results Guide Possibly the loop you run into when trying to download from PCDC is related. A colleague had the same loop issue and had to clear ...
Posted By Lesley Dec 03, 2025 01:50:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Ezobi, I think it is important to clarify what they mean with zones and conduits. In addition to what Philip mentioned, if referring to VLAN segmentation and routing, then all Stratix 5200 switches support this with static and connected routing. They also support Access Control ...
Posted By Lesley Nov 20, 2025 03:26:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Ryan, First of all, a verification of the switch configuration is a good starting point (e.g., correct use of smartports, ...). In CLI (accessible via WEBUI on Stratix 5200) you can do a 'show-tech support' command or add it to the debug bundle which can be downloaded via: Troubleshooting ...
Posted By Lesley Oct 22, 2025 02:17:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Onayli, Based on the LED status, I don't think the switch is fully booted. In that case the express setup will not work. 1. Express setup When connected via PuTTY, please verify whether the switch fully boots or where it stops? Are there any errors shown? Stopped at bootloader prompt? ...
Posted By Lesley Oct 20, 2025 08:04:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Onayli, If the express setup is not working, apart from looking at the suggestions that Philip mentioned in the technote, you can connect via a console cable (serial or usb) and monitor the CLI (e.g., via PuTTY). This way you can see what the switch is doing in the background. The express ...
Posted By Lesley Oct 17, 2025 03:54:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Onayli, Can you explain what the LED behavior was when the express setup was not working and what you did to make it work? There are 3 types of express setup: Short press (single mode) - switch assigns IP address to PC (needs to be set to automatic - DHCP) when connected to the ...
Posted By Lesley Aug 20, 2025 02:48:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Robert, The public device 200.200.200.245 (PC) requires to be translated to a unique IP address in the private range. So, you need a public to private translation of: 200.200.200.245 -> 192.168.0.x , where x is a not used address in that private space, for example 245. What happens ...
Posted By Lesley Aug 18, 2025 03:39:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Robert, Some things to bare in mind when configuring L2NAT on a Stratix 5400: Make sure you assign the NAT instance to the uplink ports on the correct VLAN (the same VLAN is used on the private and public side). When trying to access the NAT translated device from the same VLAN on ...
Posted By Lesley Apr 25, 2024 02:57:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Rivera, There are several tools available to monitor and troubleshoot an EtherNet/IP networks. Following manual is a bit older, but contains some basics of troubleshooting: Troubleshoot EtherNet/IP Networks Application Technique, ENET-AT003B-EN-P (rockwellautomation.com) What ...
Posted By Lesley Mar 12, 2024 12:12:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Prakasha, As Philip mentioned, no issue in connecting it to the device port of the ETAP. This is the intention. In your case, as the 1794-AENTR is DLR capable, it could also be directly connect into the DLR ring. I would verify whether the cable itself is correctly installed and working ...
Posted By Lesley Jan 26, 2024 07:26:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Mohmad, Please find an extract of the reference manual included in the latest released Network Device Library v12.03.00. The DLR Redundant Gateway status is being shown by the DLR faceplate. In case you would still need the message instructions for DLR, you can find ...
Posted By Lesley Jan 26, 2024 07:25:51 AM
Found In Library: Networks
Posted By Lesley Jan 19, 2024 10:35:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi James, About the REP ring, I now see you have 2 DLR rings (mistakenly thought you had 1 DLR ring). So, I assume DLR redundant gateway is enabled on those switches. In that case, no loops at that level ;-). For the connection between the switches, you do create a loop once the REP ring is operational ...
Posted By Lesley Jan 19, 2024 08:18:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi James, Did you had a chance to try any of the suggestions made previously? Based in the config files, the REP configuration has not been changed. When you have a working REP ring (verify in Device Manager), you do not need to make another connection between both switches DS1 and DS2 as this ...
Posted By Lesley Jan 18, 2024 04:35:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Matthew, In addition to the above, From Secure-rm001 - System Security Design Guidelines (rockwellautomation.com) p35 - Device Hardening Digitally signed firmware and software helps to make sure that users download and use authentic Rockwell Automation content. The ...
Posted By Lesley Jan 17, 2024 02:06:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
The linked Knowledge Base article requires you to have a TechConnect access level in order to see it. Alternatively, following CPwE design and implementation guide may assist you in understanding the REP protocol and how to set it up. Deploying a Resilient Converged Plantwide Ethernet Architecture ...
Posted By Lesley Jan 16, 2024 04:42:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Vilayil, From what I can see in another post, there has been several misconfigurations on the switches and I'm not sure what the status is now. From the picture shown, at least one of the switches has a fault (red LED OUT). You can see the fault via Monitor -> Syslog information via the ...
Posted By Lesley Aug 25, 2023 04:47:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi McKenzie, Stratix managed switches by default (OOB) have spanning tree enabled (protecting against loops). As you mentioned you went online to the switch, I assume an express setup has been performed. This also enables and configures lots of other features in the background like spanning tree ...
Posted By Lesley May 15, 2023 08:02:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Xander, Based on the input you provided earlier, my understanding is that your configuration is not correct. NAT in Stratix switches is Layer 2 NAT, meaning that the VLAN doesn't change during NAT translation, only the IP addresses as per configuration. * VLAN 2 and 99 are not needed in that ...
Posted By Lesley May 09, 2023 04:42:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Xander, MST is backward compatible with PVST+ and Rapid-PVST+. An MST switch is connected to other STP (PVST+ and Rapid-PVST+) switches by the Common Spanning Tree (CST). But you can change it if wanted. Rapid-PVST+ uses RSTP to provide faster convergence (compared to PVST). Kind regards, ...