List of Contributions

Ramgaard

Contact Details

Ramgaard


My Content

1 to 6 of 6 total
Posted By Ramgaard Sep 22, 2023 02:41:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi fuzzy logic, Thanks, The QA62129 was exactly same conclusion I got after looking into the manual . it's a bit annoying, cause Rockwell has recommended us to select Kinetix 5100 as the replacement of Kinetix 300, and on the Kinetix 300 is it possible to control the torque via the bus, ...
Posted By Ramgaard Sep 18, 2023 07:04:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, I was wondering if it's possible to make a torque limit while running the motor using MAJ. Through the PLC interface. So far have only been able to limit the torque using the I/O interface and assign two inputs for limiting the torque. It works, but it limits my flexibility. ...
Posted By Ramgaard Sep 12, 2023 10:28:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thanks fuzzy logic, this was very helpful ! It will help us move on with the project :) ------------------------------ Best Regards, Ramgaard ------------------------------
Posted By Ramgaard Sep 11, 2023 01:52:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thanks Ryan, but I actually do have that sample program. What could be nice was a description of the individual instructions provided with this AOI, like the MAT I have attached a picture from the help on the instruction, but it does not have a very good description. I can't figuring out how to ...
Posted By Ramgaard Sep 11, 2023 08:23:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, I got trouble finding the correct place for downloading AOI's from Rockwell + the documentation for the AOI. I have an AOI for the Kinetix 5100, 2.00.00 . But I want to ensure that I got the newest but have not been able to locate it anywhere. Not even the version I'm using right now. ...