Previously we used a Danfoss VLT FC51, 3 Phase, 11Kw, 23A 132F0058 In combination with this drive we used a motor with the following nameplate: Power 11 KW, 22A, 1440 RPM, 400V, Motor NP Hertz: 50 Hz. Motor Poles 4 Now we have changed this for the following motor, Motor Power Rating: 5,5 KW, ...
|