List of Contributions

*RDZ*

Contact Details

United States

*RDZ*


My Content

1 to 18 of 18 total
Posted By *RDZ* Jul 14, 2026 11:35:00 PM
Found In Egroup: Automation Control
\ view thread
Hello, I'm looking for some ideas on the best way to handle product tracking in Studio 5000 v37 for a vision inspection application. The process is pretty straightforward: a product stops at a gate, the vision system inspects it, and determines whether it needs: -No action -An orientation correction ...
Posted By *RDZ* Apr 16, 2026 01:55:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi everyone, I'm working in FactoryTalk Optix Studio and trying to replicate a solution (link below) I previously used, but with a different data source. In an earlier project, I used a dynamic link + key converter on a Panel Loader to load different screens based on the client's IP address. ...
Posted By *RDZ* Oct 01, 2025 10:49:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Ah, Thank you! That was it and I did not know that. It working like I want it to. ------------------------------ RDZ ------------------------------
Posted By *RDZ* Oct 01, 2025 09:53:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Yes, i understand that and thats what i did. However, when trying to link with the toggle button i am unable to expand the main window properties to select the variable created. ------------------------------ RDZ ------------------------------
Posted By *RDZ* Oct 01, 2025 09:41:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
@asemlucben Thank for sharing this project. I was able to test the application and it definitely what I'm looking for. However, when i try to duplicate the button actions I am unable to drill down into the Main Window Properties to select the "ScreenId" variable created. Any suggestions? ...
Posted By *RDZ* Sep 30, 2025 02:56:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
You're right, it ended up being the time on the PLC that was off. I don't know how I didn't think to check that first. Since I'm still pretty new to Optix, I assumed it had something to do with the application itself. Thanks for pointing me in the right direction. ------------------------------ ...
Posted By *RDZ* Sep 30, 2025 02:02:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi all, I'm having an issue where both my Active Alarms and Alarm History are not populating with the correct timestamps. I already verified that my Optix panel has the correct time, but the alarms are still off. Has anyone run into this before or know what could be causing the timestamp ...
Posted By *RDZ* Sep 30, 2025 01:59:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey all, I'm working in Optix and I'd like to have my navigation buttons change color or style based on which screen is currently loaded in the Panel Loader. I've assigned a variable to each screen called screenid, but I'm not sure how to link that to my key-value converter. I also have separate ...
Posted By *RDZ* Sep 23, 2025 09:46:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello All, I am interested in making a circular gauge look similar to the screenshot below. The current available circular gauge doesn't seem to have many options to make like this. If you have any recommendation, please let me know. ------------------------------ RDZ ------- ...
Posted By *RDZ* Sep 19, 2025 06:10:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
SUCCESS!!!! My dashboards are now displaying their own screens while only running 1 Optix application. My solution: instead of using the dynamic link and key-converter to replace Windows (which from what I read isn't possible). I used the dynamic link and key-converter on the Panel Loaders properties. ...
Posted By *RDZ* Sep 19, 2025 02:45:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Okay, so I went ahead and deleted my Overview Window completed and ran the project without it. See error in screenshot below. it seems the key-converter is not resolving my IPs. ------------------------------ RDZ ------------------------------
Posted By *RDZ* Sep 19, 2025 01:40:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
@AutomateSHANE Thank you for expanding on this and including the project file. That really cleared things up and it's definitely something I want to replicate. I set up my project in a similar way, but I'm getting some errors, and it isn't working as intended. See screenshot below. Both my dashboards ...
Posted By *RDZ* Sep 18, 2025 02:32:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
@AutomateSHANE This seems more like what I'd like to do. All my clients have static IPs, so that part shouldn't be an issue. I understand the idea of using the key value converter, but what I'm not clear on is how to actually tie the IPs to their corresponding screens. I tried looking for the (Session) ...
Posted By *RDZ* Sep 16, 2025 12:54:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I had the same thought initially, but when I tried it out Optixs didn't allow me to create more than one Native Presentation or more than one Web Presentation. I can create multiple main windows, but that's it. After doing some more searching online, it looks like the only option is to build an overview ...
Posted By *RDZ* Sep 16, 2025 10:43:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks for clarifying. Based on what you said, I think it makes the most sense for us to keep a single runtime and just design different screens for the different use cases. What I'm not clear on is how to set up each client so they only see the screens that apply to them. Is there a way to configure ...
Posted By *RDZ* Sep 16, 2025 09:39:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello All, My main question is about running multiple Optix applications on the same server. I created an Optix application that is running on a server and I purchased a 21 token package for it. I don't think all of them were used, maybe around 7-10. I just wasn't sure how many I would need to start ...
Posted By *RDZ* Dec 11, 2023 10:48:00 PM
Found In Egroup: Automation Control
\ view thread
GLaDOS, Your assistance has been very helpful in aligning my understanding. Your explanation bridged the gap between my initial thoughts and practical implementation. Our object scan time ranges between 120 - 450ms, with expected max peaks fluctuating from 1 to 5. Our ultimate goal involves determining ...
Posted By *RDZ* Dec 11, 2023 10:59:00 AM
Found In Egroup: Automation Control
\ view thread
Hi everyone, I'm working on a project that involves using a Keyence LR-X100 sensor in Studio 5000 V35 ladder logic to determine the maximum height of an object, detect when it reaches its peak and count the max peaks of the object. Any insights, sample logic structures, or advice on utilizing Rockwell ...