List of Contributions

shachar

Contact Details

shachar


My Content

1 to 4 of 4 total
Posted By shachar Feb 08, 2023 10:55:00 PM
Found In Egroup: Automation Control
\ view thread
I tried "\my documents" and it worked - thank you very much. I have another question, is it possible to save the files to a folder accessible via FTP? So that I can access the files from a remote computer without having to access in VNC. ------------------------------ shachar -------------- ...
Posted By shachar Feb 07, 2023 02:03:00 AM
Found In Egroup: Automation Control
\ view thread
To generate the alarm history.CSV at runtime I change the firmware to 12.0. I have defined the CSV SETUP in the project. But when I run the trigger I can't find a generated CSV file. attached the CSV SETUP. ------------------------------ shachar ------------------------------
Posted By shachar Feb 05, 2023 08:58:00 AM
Found In Egroup: Automation Control
\ view thread
PanelView Plus 7 Perf 1200W Revision 8.001 SN 00CB2250 How do I get the alarm history LOG file out of a Panelview Plus 7? I would like to upload the fault history from the panel to the PC, if it is possible to transfer the file to CSV format or import it to Excel. I can connect to the panel ...