List of Contributions

Aldair Ribeiro

Contact Details

Aldair Ribeiro


My Content

1 to 20 of 25 total
Posted By Aldair Ribeiro Mar 25, 2026 10:13:00 AM
Found In Egroup: Advanced Software
\ view thread
Updating here to help anyone who might encounter this problem in the future. 1- I managed to resolve the "Failed to get configuration" error after enabling port fast on the switch and Rapid spanning-tree. When you turn on the Thin Client 6300B, it connects to the switch, and the switch takes about ...
Posted By Aldair Ribeiro Mar 02, 2026 05:28:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, We updated our thin manager from version V13.1 to 14.1 and we have some 6300T-BA thin clients. I'm using the USB touchscreen driver. When the thin client is initialized, it doesn't recognize the touchscreen. To get it working, I need to reconnect and reconnect the USB cable between ...
Posted By Aldair Ribeiro Feb 20, 2026 09:20:00 AM
Found In Egroup: Advanced Software
\ view thread
Adam, thank you for the quick reply. I'm using the licenses in FactoryTalk Activate Manager, but I'll try installing directly on the Thin Manager. I don't run View Studio; I'm using GE's iFix. "When you first launch the ThinManager console on the host, does it report any errors that seem erroneous?" ...
Posted By Aldair Ribeiro Feb 20, 2026 05:08:00 AM
Found In Egroup: Advanced Software
\ view thread
We are updating our thin client environment. We migrated from V13 (Windows Server 2012) to V14.1 running on new redundant servers with Windows Server 2025 Standard. Currently, we operate with 13 terminals (9 VersaView 6300T-BA units and 4 Advantech Industrial PCs). Despite the migration, we are facing ...
Posted By Aldair Ribeiro Feb 13, 2026 08:28:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello, I have Thin Manager licenses, and the license document shows that they are for version 13.01.00 (Thin Manager FTA 1 VFLX ESD PS/W). My question is: can I use this license with a Thin Manager version 14.00 without upgrading the license? Sincerely, -------------------------------------- ...
Posted By Aldair Ribeiro Jan 07, 2026 08:48:00 AM
Found In Egroup: Advanced Software
\ view thread
I'm trying to update the firmware package of a 6300T-BA thin client that was on version 9.5 because the Thin Manager version is 14.01 build 14000. I downloaded the package from the Thin Manager website. I installed it, but I noticed that it doesn't update the bootloader version. When the thin client ...
Posted By Aldair Ribeiro Oct 30, 2025 08:58:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, good morning! In an environment with 2 redundant SCADA servers, using the same server for the Thin Manager and having 12 thin clients connected, do I need to install 12 CALs on each server or just 12 on one of them? Regards, -------------------------------------------
Posted By Aldair Ribeiro Sep 08, 2025 06:22:00 AM
Found In Egroup: Advanced Software
\ view thread
I'm having a problem with Thin Manager v13.2 on Windows Server 2012. ThinServer is running, and my 9 clients are connected. However, I can't open the Thin Manager interface. It opens, but then freezes, and I can't do anything else. I noticed that the Thin Module is consuming 7GB of memory. Is there ...
Posted By Aldair Ribeiro Sep 05, 2025 07:37:00 AM
Found In Egroup: Advanced Software
\ view thread
Thanks Adam, greetings from Brazil! Since it's compatible with Server 2022, is that a guarantee that it will be compatible with 2025? Apparently, Rockwell hasn't declared compatibility yet.-------------------------------------------
Posted By Aldair Ribeiro Sep 03, 2025 06:10:00 AM
Found In Egroup: Advanced Software
\ view thread
I currently have Thin Manager V13.2 running on Windows Server 2012 Foundation with 15 clients. We're replacing this server with one running Windows Server 2025 Standard. I haven't found any Rockwell documentation that mentions compatibility between the two. Has anyone used it? -------------------- ...
Posted By Aldair Ribeiro Oct 14, 2024 07:28:00 AM
Found In Egroup: Installation & Activation
\ view thread
I'm trying to install Connected Components Workbench V22 and the installation won't go beyond 15% (starting the Microsoft Visual Studio 2015 Shell installer). Does anyone have a solution? Another question... I need to program a 2080-L50E24QBB. Before installing V22 I tried V12 and there was no option ...
Posted By Aldair Ribeiro Jul 24, 2024 04:14:24 PM
Found In Library: Automation Control
Posted By Aldair Ribeiro Jul 24, 2024 04:14:00 PM
Found In Egroup: Automation Control
\ view thread
Hello! I have a 1794-IE8H module controlled by a 1756-L71 and 1794-AENTR CPU. I want to read the signal from a pressure sensor that transmits 4-20 mA. However, I would like to obtain maximum resolution from the module - the application is measuring the level of a tank per column. - for this I configured ...
Posted By Aldair Ribeiro Jun 24, 2024 07:13:00 AM
Found In Egroup: Advanced Software
\ view thread
Good morning! I have two servers SLK1500P and SLK1500S both are on the same network and run Windows server 2012 Foundation. On the SLK1500P I have 9 thin clients connected and running perfectly. I'm trying to enable redundancy and the message "RPC server is not available" error "800706ba" appears. ...
Posted By Aldair Ribeiro Jun 10, 2024 11:32:00 AM
Found In Egroup: Advanced Software
\ view thread
I have 8 thin clients connected to my server and managed through thin manager. After activating the screen saver I noticed that communication was unstable, the error log shows several communication losses. By removing the screen module the problem was removed, however it is an animation that agreed with ...
Posted By Aldair Ribeiro Aug 18, 2023 03:11:22 PM
Found In Library: Networks
Posted By Aldair Ribeiro Aug 18, 2023 03:11:00 PM
Found In Egroup: Networks
\ view thread
I am sending print of ENI Utility ------------------------------ Aldair Ribeiro ------------------------------
Posted By Aldair Ribeiro Aug 18, 2023 03:10:00 PM
Found In Egroup: Networks
\ view thread
Hello Ryan! 1-I'm trying both google chrome and internet explorer (MS edge) . 2-The TX/RX light blinks normally at high frequency. 3-I'm just turning off the ENI. 4-The firmware version is already 3.22. In a last test carried out today I noticed that the direct communication ...
Posted By Aldair Ribeiro Aug 17, 2023 06:33:00 AM
Found In Egroup: Networks
\ view thread
Edited to translate into English. Please post in English going forward. @Aldair Ribeiro. Thank you. -EF EDIT: corrected Original Message View by HTML source code -FL No parameters are shown on the webpage and I also don't have access to the error log as shown in the manual. - ...
Posted By Aldair Ribeiro Aug 17, 2023 06:32:00 AM
Found In Egroup: Networks
\ view thread
------------------------------ Aldair Ribeiro ------------------------------