List of Contributions

Fishbinder

Contact Details

Fishbinder


My Content

1 to 3 of 3 total
Posted By Fishbinder Apr 12, 2024 09:42:00 AM
Found In Egroup: Automation Control
\ view thread
Philip, Thanks for the suggestion but it seems that the problem was a rather silly bug in the original program. The EntryStatus returned from the GSV command was compared with wrong mask value that included bits that are not part of the comm status of the 20-comm-e interface. I changed the Mask and ...
Posted By Fishbinder Apr 11, 2024 08:00:12 PM
Found In Egroup: Automation Control
\ view thread
HI Philip, It seems that even if I match the module and upload from the drive while offline I cannot get the drive comm to connect. I tried several tricks like closing the project, etc but I can't seem to clear the comm fault. This must be something silly that I'm overlooking. Resetting the module ...
Posted By Fishbinder Mar 29, 2024 08:37:00 PM
Found In Egroup: Automation Control
\ view thread
I updated a L61 CPU to a L81E and also upgraded from Logix 5000 V17.0 to V30 on a system with a 700S 2 drive , 20-comm-E adapter and 700V drive. When I changed controllers and upgraded the application I added the AOPs for the drive. I downloaded into the controller in a standalone rack before i was onsite. ...