List of Contributions

DAVID PERGANDE

Contact Details

DAVID PERGANDE


My Content

1 to 6 of 6 total
Posted By DAVID PERGANDE Apr 29, 2025 07:47:00 AM
Found In Egroup: Automation Control
\ view thread
Will do Thanks, David
Posted By DAVID PERGANDE Apr 29, 2025 03:22:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you for the response. So if I read documentation correctly, I will have 1 SIL2 task set at priority 1 with 1715 AOIs only, with 1 additional task MainTask set at priority 2 for all logic. Similar to attached
Posted By DAVID PERGANDE Apr 24, 2025 08:57:00 AM
Found In Egroup: Automation Control
\ view thread
I am adding SIL2 functionality to an existing applicaiton. I am adding 1715 IO to an existing 1756-L75. The Current application has only 1 MainTask (under tasks) setup as Priority 1. In relation to 1756-RM001T-EN-P - August 2023, page 95. that SIL2 should have a dedicated task, set to priority 1. All ...
Posted By DAVID PERGANDE Dec 16, 2022 08:01:00 AM
Found In Egroup: Automation Control
\ view thread
EDIT: moved to Automation Control community -FL What are the best ways to prevent unauthorized access to a standalone (not connected to a network) 1769-L30ER. Thanks, David ------------------------------ DAVID PERGANDE ------------------------------
Posted By DAVID PERGANDE Dec 16, 2022 07:40:00 AM
Found In Egroup: Automation Control
\ view thread
EDIT: corrected typo in title and moved to Automation Control community -FL Is there a way to disable either the USB or Ethernet ports on a1769-L30ER? I assume not? Thank you, David ------------------------------ DAVID PERGANDE ------------------------------