List of Contributions

Julia

Contact Details

Julia


My Content

1 to 20 of 35 total
Posted By Julia Apr 29, 2026 03:41:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello @Ramakrishnan I have one suggestion that might help, although I'm not sure if it would fit your application. If it is not important for the operator to view alarms from other areas, you could create one Alarm Summary screen for each area. Then, based on the user group, you can create logic ...
Posted By Julia Oct 16, 2025 11:04:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello everyone, I'm currently working with FT View SE integrated with DataLogProPlus Service, which is hosting an embedded InfluxDB instance for data historization. The configuration is working correctly - I've already: Created the Influx database through the DataLogProPlus; Verified that ...
Posted By Julia Aug 12, 2025 09:30:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Morrison, a few things I thought might help in your case: Review the speed loop tuning: Parameters such as P52 [Spd Reg Kp] and P53 [Spd Reg Ki] can amplify small variations. A high gain ratio will speed up the response but can also introduce oscillations. If you can test, Try lowering the Speed ...
Posted By Julia Aug 08, 2025 10:09:00 AM
Found In Egroup: Advanced Software
\ view thread
Ótimo Marcel, Muito obrigada pela resposta. Entendi e concordo com os pontos que você colocou sobre seguir a ISA 18.2, evitar múltiplos níveis adicionais de alarme no processo. No entanto, neste projeto, esses alarmes adicionais já constam na documentação do cliente e fazem parte de intertravamentos ...
Posted By Julia Aug 07, 2025 12:16:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi everyone, I'm currently using the PlantPAx v5.20.01 process library and came across a situation where some instruments in my project require more than 4 analog alarm limits, which goes beyond the standard HH, H, L, and LL available in blocks like PAI. Here is a real example from my project (see ...
Posted By Julia Jul 18, 2025 12:47:00 PM
Found In Egroup: Advanced Software
\ view thread
I wanted to circle back and clarify one thing, as I realized my original message might have given the impression that latched alarms are rare. In fact, it's quite the opposite in the systems I've worked with. In most offshore platforms I've been involved in, latched alarms were the default behavior ...
Posted By Julia Jul 18, 2025 10:29:00 AM
Found In Egroup: Advanced Software
\ view thread
In most of the cases I mentioned, the operator interacts with latched alarms through the standard PlantPAx faceplates, using the built-in "Acknowledge and Reset" buttom available in faceplate object from PlantPAx library. These are intuitive and work well. To make things clearer for the operator, ...
Posted By Julia Jul 18, 2025 08:54:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Chris, Speaking from experience, I've seen several real-world cases where latching the alarm made a big difference. One example was on an offshore platform, involving thermal protection thermistors on water injection pump motors. The temperature would briefly exceed the limit, triggering an interlock, ...
Posted By Julia Jul 15, 2025 12:48:00 PM
Found In Egroup: Automation Control
\ view thread
There is not really an adapter that lets you turn a CompactLogix rack into remote I/O for a ControlLogix processor. CompactLogix just was not designed to work that way. Unlike ControlLogix, where you can drop in an EN2T or similar module in a remote rack, CompactLogix doesn't support being used as a ...
Posted By Julia Jul 15, 2025 12:24:00 PM
Found In Egroup: Advanced Software
\ view thread
If EmulateEthernet still shows the device as "Unknown", open Studio 5000 Logix Designer, go to Communications > Who Active, and check if the controller shows up under the Emulate path. As an alternative, you can create the virtual controller in FactoryTalk Logix Echo directly from the .ACD file, this ...
Posted By Julia Jul 11, 2025 09:35:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Michael, I use the FactoryTalk Diagnostics Viewer to monitor the Directory's behavior. You can filter for messages related to the FactoryTalk Network Directory and check for token resolution issues or sync failures. I also check the Windows Event Viewer on the Directory VM under "Rockwell Software ...
Posted By Julia Jul 11, 2025 08:32:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Lawrence, You're totally right the MSG instruction does check .DN and .ER on its own, and won't retrigger if one of them is still active. But in practice, I've seen cases where just checking .EN = 0 isn't enough. If the logic is more spread out or if something resets the MSG tag elsewhere, it might end ...
Posted By Julia Jul 10, 2025 02:47:00 PM
Found In Egroup: Advanced Software
\ view thread
For item 1, the "Effective Permissions" are checked in the Security Settings of each HMI server within FactoryTalk Administration Console. You can right-click the area (or server) where the issue occurs, go to Properties > Permissions > Effective Permissions, select the user or group (like Area01_Advanced), ...
Posted By Julia Jul 10, 2025 09:25:00 AM
Found In Egroup: Advanced Software
\ view thread
ah, now I get it! The Navigation Menu in FactoryTalk View SE is designed to be structured by areas and subareas, not individual screens. That means you should organize your displays in folders that represent each process area, and then assign those entire folders to the navigation menu - not individual ...
Posted By Julia Jul 10, 2025 08:45:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Michael, Here are some suggestions to help: Check "Effective Permissions" in FactoryTalk Administration Console for the affected tags and user group. There may be inherited deny rules at specific tag or area levels. Disable automatic logout in Runtime Security settings. Silent logoffs ...
Posted By Julia Jul 10, 2025 08:19:00 AM
Found In Egroup: Advanced Software
\ view thread
Gabriel, Just to make sure I'm understanding right: you're expecting the navigation menu to automatically highlight the current screen when it first opens, even if that screen wasn't selected through the menu? Also, are you using the WebNavigation feature (the one that auto-generates the side menu ...
Posted By Julia Jul 09, 2025 12:25:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
GRO, here are some direct points based on the ENET-UM527-EN-P manual (EtherNet/IP Socket Interface): Which attribute did you use in the SetAttributeSingle? Please confirm if it was Attribute 4 (RecvBufSize). That's the one that sets the receive buffer size. (From Table 16 Manual) Trigger ...
Posted By Julia Jul 08, 2025 03:38:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Hi GRO, Try triggering the UDP MSG Read continuously, not just on a timer or event. Use the .DN bit of the previous MSG to fire the next one. If you let the MSG overlap or leave gaps, the EN2T might buffer the packet and delay delivery to the PLC exactly what you are seeing. Also: Make sure ...
Posted By Julia Jul 08, 2025 03:19:00 PM
Found In Egroup: Automation Control
\ view thread
Hi Wagner, You're right - Studio 5000 doesn't support Undo (Ctrl+Z) when editing tag lists. If you delete or overwrite something, there's no way to undo it. Undo works fine inside routines like Ladder or Structured Text, but unfortunately not in the tag editors. What I usually do is export the data ...
Posted By Julia Jul 06, 2025 06:24:00 PM
Found In Egroup: Automation Control
\ view thread
You're totally right, it's really unlikely that three identical 1794-OE4 modules would all have the same exact issue just by coincidence. Since all 12 channels are showing the same 0.35 mA deviation, and you've confirmed it happens at both 4 mA and 20 mA directly on TB3, this doesn't look like a random ...