List of Contributions

Alfredo Pereira

Contact Details

Alfredo Pereira


My Content

1 to 5 of 5 total
Posted By Alfredo Pereira Nov 26, 2024 09:54:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, everyone! I'm having a problem when importing control strategy routines from the Process Library 5.2. Can anyone help me understand or resolve this error?
Posted By Alfredo Pereira Oct 01, 2024 11:16:00 AM
Found In Egroup: Networks
\ view thread
Hello guys, Is it possible to connect multiple drives in a DeviceNet trunk network using a daisy-chain configuration? I plan to connect 15 drives and one remote, and the total cable length is about 100 meters. Will this setup work reliably, or should I consider an alternative topology like trunk ...
Posted By Alfredo Pereira Apr 06, 2022 09:17:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello Ronald. Thanks for reply. But i would like know If is possible the operator jump the step or go to back manually, Due to the need of the process.
Posted By Alfredo Pereira Apr 06, 2022 09:10:00 AM
Found In Egroup: Advanced Software
\ view thread
How I configure this? Conserve system resources, limit the total number of displays in the cache to 40. This includes displays loaded using this option or using the Display /Z or /ZA command. Also, limit the number of displays that are displayed or minimized simultaneously to 40.
Posted By Alfredo Pereira Mar 31, 2022 12:23:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello. Someone know if is possible go to back or jump steps by comand, inside sequence steps using (P_Seq V3.5 ProcessLibrary)?