List of Contributions

Teti

Contact Details

Teti


My Content

1 to 17 of 17 total
Posted By Teti Nov 29, 2021 09:17:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you for the reply. I was sure of those variables being READ/WRITE. ------------------------------ Teti ------------------------------
Posted By Teti Nov 29, 2021 01:36:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, sorry for the late reply. I've got the FactoryTalk View Studio 11.00.00 (CPR 9 SR 11) and FactoryTalk Linx 6.11.00 (CPR 9 SR 11.0). ------------------------------ Teti ------------------------------
Posted By Teti Nov 26, 2021 09:55:00 AM
Found In Egroup: Automation Control
\ view thread
Those are the variables Implemented in the PLC. I'd like to identify different regions of the display on which a user the select ITEMS. I could do that by adding for each item a different BOOL, so that the PLC know which one is active and which don't, but I thought it could be done more smart by using ...
Posted By Teti Nov 26, 2021 09:47:00 AM
Found In Egroup: Automation Control
\ view thread
Ok, I've tried creating the DINT variable and it works, both the displaying as well as the button writing the value. Now I have to figure out why it doesn't work with a UINT value and how do I manage to use multiple buttons writing different values to the same area. What do you suggest now ? ...
Posted By Teti Nov 26, 2021 09:22:00 AM
Found In Egroup: Automation Control
\ view thread
For now I'm using the Test Display to test the interface I'm Building. I made a simple momentary button: State0 has a 0 value. While State1: In the connections I've put the TAG by searching it in the TAG Browser, as mentioned: I've tried using a different variable with the same result. I ...
Posted By Teti Nov 26, 2021 09:11:00 AM
Found In Egroup: Automation Control
\ view thread
I've removed the space from my post but since I used the TAG BROWSER, I didn't add a space in the value assignment. So it wasn't what caused my error. Not fixed yet :( Would there be problems if multiple buttons write the same INTEGER? ------------------------------ Teti -------------------- ...
Posted By Teti Nov 26, 2021 08:57:00 AM
Found In Egroup: Automation Control
\ view thread
I've used the Tag Browser for the selection of the correct TAG. Sorry for the unwanted space. I've also fixed my previous post. ------------------------------ Teti ------------------------------
Posted By Teti Nov 26, 2021 08:32:00 AM
Found In Egroup: Automation Control
\ view thread
I thought about that too but I get erros if I have it configured, just like yours, and I put ([PLC) VARIABLE_INT) in the Connections -> Value. The messages are : Write attempt for item '([PLC)VARIABLE_INT)' failed (configuration error) Problem writing value '0' to item '([PLC)VARIABLE_INT)' What ...
Posted By Teti Nov 26, 2021 07:59:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, for starter, thanks again for the support you are giving me. I'm back with a different kind of problem from the previous ones. I am now working on a HMI interface and I'm using the official FactoryTalk View Studio. I'd like to create a button(momentary, maintained,.... ) that when clicked ...
Posted By Teti Nov 11, 2021 05:03:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you for your reply. I managed to make the code I had working. It works the first time I run it and have issues on the following ones, meaning that I can't read multiple times because the READ moves to ERROR states. This code seems better because it can even reestablish the connection to the ...
Posted By Teti Nov 05, 2021 02:24:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you for your reply! I know I use the same TAGS in the MainRoutine and in Test. I've copied the code from the MainRoutine in Test and applied my modification, like avoiding the Delete_Istance. Sorry for my question but how can you write an IP like 192.168.0.10 into a DINT Variable of 32 bit without ...
Posted By Teti Nov 05, 2021 02:17:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you for your reply! I've tried to configure the port which has the Ethernet cable plugged in, by clicking browse in every MSG command and selecting the correct A1, Ethernet. The system always change it to "THIS". Even though our company has the Contract, my account can't seems to recognize it ...
Posted By Teti Nov 04, 2021 04:22:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you! That was something I didn't know was possible :) ------------------------------ Teti ------------------------------
Posted By Teti Nov 04, 2021 04:01:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, I'm also trying to establish a Modbus TCP communication between a 5069-L310ER and another PLC. The Allen-Bradley will work as a Master while the other PLC will work as a Slave. I've downloaded the example provided in the support at https://rockwellautomation.custhelp.com/app/answers/answer ...
Posted By Teti Nov 04, 2021 04:00:43 AM
Found In Library: Automation Control
Posted By Teti Nov 04, 2021 03:33:00 AM
Found In Egroup: Automation Control
\ view thread
Hello everyone, I'm new here and I'm already in need of help. I'm trying to establish a basic TCP/IP communication between a Rockwell PLC 5069-L310ER and an embedded PC. What I'm trying to do is to read the stream of data from the embedded PC which consists of a stream Strings packet of JSON. I've ...
Posted By Teti Nov 04, 2021 03:32:58 AM
Found In Library: Automation Control